AutomationDirect.com - The common sense way to buy industrial controls. 1-800-633-0405   AutomationDirect.com - The common sense way to buy industrial controls. 1-800-633-0405AutomationDirect.com - The common sense way to buy industrial controls. 1-800-633-0405
Click here to view your shopping cart.
Cart Total
$0.00  

Product Lines
Other site information from AutomationDirect FREE online Seminars FREE online tech support Get your copy of our latest product information in print for handy reference
Home Tech Support Downloads Product Info Documentation About Us My Account
Search
Site Map | Email Us | Contact us
Help | Business Policies |
1-800-633-0405
Our offices will be closed Friday, July 3rd, in observance of Independence Day
UPS shipped orders placed by 6:00PM ET on Thursday, July 2nd, will ship same day (if paid by Credit Card or PO account in good standing). Other shippers & drop-shipped items have earlier cutoffs (see shipping policies for details). Orders placed after the cutoff, will process on Monday, July 6th.
You are looking at:  Operator Interfaces > C-more Micro-Graphic Panels > C-more Micro-Graphic Panel Programming S/W & Cables

Products Overview Technical Info Manuals Reviews
 
Categories:  C-more Micro-Graphic Panels & Keypad Bezels (all types)  C-more Micro-Graphic Panels & Keypad Bezels (3 inch only)  C-more Micro-Graphic Accessories (3 inch only)  C-more Micro-Graphic Panels & Keypad Bezels (6 inch only)  C-more Micro-Graphic Accessories (6 inch only)  C-more Micro-Graphic Panel Programming S/W & Cables  C-more Micro-Graphic Panel Documentation  

Shop for this product


C-more Micro-Graphic Panel Programming Software and Cables

HMI touch panels at a text panel price!

[Jump Down to Cables]
C-more Micro-Graphic Panel Programming Software is a spin-off of its powerful sibling, the C-more Touch Panel. C-more Micro software offers very high end features designed to reduce your configuration time.
  • Simply drag and drop the objects from the object bar (right side of screen) onto the screen construction area.

  • Then configure your PLC tags and click on the objects you wish to use.

  • Use the built-in simulator to review your work on your PC before ever downloading your project!
The time saving benefits of the C-more configuration software could easily pay for the panel.

Learn more. Visit www.C-moreMicro.com for detailed specifications, a virtual tour of the product, programming examples, newest communication drivers, and more.
C-more Micro-Graphic Panel Programming Software
Free! ... C-more Micro-Graphic Panel Software

Download now or purchase a CD version for $25.00 (EA-MG-PGMSW).
Complete C-more Micro Software Overview



Software Highlights
C-more Micro-Graphic Programming Software

Built-in project simulator

  • Runs your project on your PC
  • Test all of your screens before downloading
  • Time savings pays for the panel!

Built-in user object/screen libraries

    Save time by re-using your custom objects and screens.

Thumbnail project preview pane

    Helps keep track of multi-screen projects.

Scrolling Object selection window

    Lets you find the object you want fast. Just drag and drop it on the screen.

Scrolling help window

    Gives you helpful information on each object.
C-more Micro-Graphic Panel Objects

C-more Micro-Graphic line object Line - allows the user to insert a straight line drawing into a project. Micro-Graphic rectangle Rectangle - allows the user to insert a drawing of a rectangle as well as other geometric shapes into a project.
C-more Micro-Graphic circle Circle - allows the user to insert a drawing of a circle or ellipse shape into a project. C-more Micro-Graphic frame Frame - allows the user to insert a Frame to the project that can be used to Frame other objects.
C-more Micro-Graphic pushbutton Pushbutton - is available from the Button Category of the Object List window. The Pushbutton object is an electronic version of a typical pushbutton normally found on control panels. C-more Micro-Graphic switch Switch - is an electronic version of a typical switch that normally can be found on control panels.
C-more Micro-Graphic indicator button Indicator Button - is available from the Button Category of the Object List window. The Indicator Button object is an electronic version of a typical indicatorbButton normally found on control panels. C-more Micro-Graphic indicator light Indicator Light - is an electronic version of a typical indicator light normally found on industrial control panels.
C-more Micro-Graphic indicator light Graphic Indicator Light - is a more enhanced version of the “Indicator Light Object” that allows the user to choose more detailed graphics to display the status of a tag. C-more Micro-Graphic numeric display Numeric Display - consists of a frame that displays a real-time numeric value according to the value data received from an assigned Tag Name.
C-more Micro-Graphic numeric entry Numeric Entry - is used to enter a value from your Panel to a PLC Register. C-more Micro-Graphic Inc/Dec value Increment/Decrement Value - is used to add or subtract a value by pressing a button on the Panel.
C-more Micro-Graphic bar meter Bar Meter - is used to monitor one or two assigned Tag Names continuously. C-more Micro-Graphic bitmap button Bitmap Button - offers the ability to use a Bitmap graphic to perform the functions of a Button. This allows users to create their own graphics and implement them within the software project.
C-more Micro-Graphicstatic bitmap Static Bitmap - offers the ability to display a Bitmap graphic on any screen. The Static Bitmap does not change state. C-more Micro-Graphicdynamic bitmap Dynamic Bitmap - offers the ability to make an object using two different Bitmap graphics that will display one graphic when the Tag is ON and a different graphic when the Tag is OFF.
C-more Micro-Graphic recipes Recipe - make it easy to make a large number of tag changes with the push of a single button. C-more Micro-Graphic static text Static Text - is used to display a Frame with a personalized Message.
C-more Micro-Graphic lookup text Lookup Text - is used to display a Frame with a Message from a lookup database. C-more Micro-Graphic dynamic text Dynamic Text - is used to display text that is retrieved from data stored in a Tag.
C-more Micro-Graphicscreen change pushbutton Screen Change Pushbutton - is a pushbutton object that can be configured to activate another screen in the project. C-more Micro-Graphic screen selector Screen Selector – is an enhanced version of the Screen Change pushbutton.
C-more Micro-Graphic adjust contrast Adjust Display Contrast - is used to allow the operator to adjust the Panel Display Contrast. C-more Micro-Graphic function Function - is used to assign the panels function key buttons to a particular action as well as assigning the control of the LED ON/OFF status.


Minimum System Requirements

  • USB port for project transfer from software to panel
  • Personal Computer with a 333 MHz or higher processor (CPU) clock speed recommended; Intel® Pentium/Celeron family, or AMD® K6/Athlon/Duron family, or compatible processor recommended
  • Keyboard and Mouse or compatible pointing device
  • Super VGA color video adapter and monitor with at least 800 x 600 pixels resolution (1024 x 768 pixels recommended) 64K color minimum
  • 150 MB free hard-disk space
  • 128 MB free RAM (512 MB recommended)
  • CD-ROM or DVD drive for installing software from the CD or internet access to download
  • Operating System - Windows® XP Home / Professional Edition with Service Pack 2, Windows® 2000 with Service Pack 4 or Windows® Vista
NOTE: C-more Micro-Graphic panels offer next generation features and because of this, the new programming software does not convert older EZText or Optimate projects.

PC Programming Connections

For project development, the C-more Micro-Graphic panel is connected to a PC USB port using the EA-MG-PGM-CBL cable assembly.

The cable assembly includes:
  • USB cable – type A and type B connectors
  • USB to RS232 converter
  • RS232 cable – RJ12 connectors both ends
The programming PC to Micro-Graphic panel connections are:

C-more Micro-Graphic to programming PC connection
  1. Connect the USB programming cable from a type A USB port on the PC to the USB type B port on the converter.
  2. Next connect the serial programming cable from the converter’s RJ12 port to the panel’s RJ12 serial port.
  3. The panel receives power from the USB port of the PC that it is connected to through the USB to RS-232 converter assembly.

C-more Micro-Graphic Power Connections

During Programming:

The C-more Micro-Graphic panel is powered from the PC through the USB to RS-232 Programming Cable Assembly, EA-MG-PGM-CBL.

C-More Micro-Graphic Panel Programming and Communication Cables

Available cables for the C-More Micro-Graphic Panels include:

PC Programming Connections
  • EA-MG-PGM-CBL - USB to RS-232 Programming Cable Assembly
Cables for direct connect to panel’s serial port 1 (Powered from PLC serial port.)
  • DV-1000CBL - Direct LOGIC PLC RJ-12 port, DL05, DL06, DL105, DL205, D3-350, D4-450 and H2-WinPLC (RS-232C).
  • D4-1000CBL - Direct LOGIC DL405 PLC 15-pin D-sub port, DL405 (RS-232C).
  • FA-15HD - Direct LOGIC (VGA Style) 15-pin port, DL06, D2-250 (250-1), D2-260 (RS-232C). Use with DV-1000CBL cable.
  • FA-CABKIT - Direct LOGIC PLC 15-pin D-sub port, DL405 (RS-232C). Use with DV-1000CBL cable.
Cables for direct connect to panel’s serial port 1 (Powered from DC power adapter.)
  • OP-3CBL-1 - Direct LOGIC PLC RJ-11 port, D3-340 (RS-232C).
Cables used with optional serial port 2 (Not powered from PLC serial port.)
  • EA-2CBL - Direct LOGIC PLC RJ-12 port, DL05, DL06, DL105, DL205, D3-350, D4-450 and H2-WinPLC (RS-232C).
  • EA-2CBL-1 - Direct LOGIC (VGA Style) 15-pin port, DL06, D2-250 (250-1), D2-260 (RS-232C).
  • EA-3CBL - Direct LOGIC PLC RJ-11 port, D3-340 (RS-232C).
  • EA-4CBL-1 - Direct LOGIC DL405 PLC 15-pin D-sub port, DL405 (RS-232C).
  • EA-4CBL-2 - Direct LOGIC PLC 25-pin D-sub port, DL405, D3-350, DL305 DCU and all DCM’s (RS-232C).
[Back to Top]

NOTE: For more details, select the "Products" tab and click on the desired "Item Code", or select the "Technical Info" tab.


Shop for this product
Shopping Tips



For payment options we accept VISA, MasterCard, Discover, American Express, I-Checks, or company purchase orders.
SecurityMetrics Credit Card Safe

Comments and suggestions: store@automationdirect.com | Order Assistance/Sales: sales@automationdirect.com | Phone Contact: (800) 633-0405
Copyright © 1999-2009 Automationdirect.com. ALL RIGHTS RESERVED. Privacy Statement

Site Map
(web3 - adc_bravo - Production Build)