This is the printable version of: http://www.automationdirect.com/adc/Overview/Catalog/Operator_Interfaces/C-more_Touch_Panels/C-more_Touch_Panel_Options_-a-_Accessories
Please note: Some pages may look best printed in "Landscape" orientation.Restore Layout
Accessories for C-more® Operator Interface Touch Panels
Available options and accessories for C-more operator interface touch panels include the following.
For All C-more Panels - Base and Full Feature
AC Power Adapter
The optional EA-AC AC Power adapter attaches to the rear of the C-more touch panel, accepts 120 VAC and provides 24 VDC power
to the panel.
The AC power adapter provides some features that a normal DC power supply can not provide. The adapter incorporates power
loss detection which signals the panel in the case of a power interruption which allows the panel to sequentially stop all logging to USB and
Compact Flash devices and shut-down before all power to the panel is lost. This helps reduce the chance of logging data being lost.
The EA-AC also allows the panel to set an error flag that can be used to log power interruptions with a time and date stamp.
The AC adapter adds about 1.5 inches to the overall depth of the panel.
[more info]
Standard USB Flash Drive
C-more can use any standard USB flash drive or "pen drive" to log PLC data, alarms, messages, etc. AutomationDirect
carries the 2GB SDCZ4-2048-A10 USB pen drive for use with C-more touch panels.
[more info]
Communication Port Adapter
The EA-ADPTR-4 adapter plugs into the 15-pin serial port on the rear of the panel to allow a PLC communication cable to be plugged in at a 90 degree angle to reduce panel depth requirements. [more info]
D-Sub 15 Pin to Terminal Block Adapter
The EA-COMCON-3 adapter is plugged into the 15-pin serial port on the rear of the panel to allow wire terminal connections for RS-422/485 PLC communication cable. [more info]
Non Glare Screen Cover
The Non Glare Screen Cover is a protective overlay used to protect the touch screen while helping to reduce glare from external light sources. [more info]
For Full Feature C-more Panels (only)
Compact Flash Card
C-more panels accept standard Compact Flash (CF) cards. You can copy projects to CF cards at your PC (no panel required), and be able to perform field updates in seconds. This is a great way to update multiple panels, or panels at remote locations. Use a CF card to log PLC data, and/or store screen captures of the panel when alarm conditions are met, or at periodic intervals. [more info]
Expansion Assembly
The EA-EXP-OPT Expansion Assembly attaches to the back of the C-more touch panel and provides two expansion slots, one for
the optional Compact Flash Card Interface Module and the other for future option modules. [more info]
CF Expansion Module
The C-more EA-CF-IF Compact Flash Card Interface Module is used with the Expansion Assembly and accepts a compact flash card,
such as the Compact Flash Memory card, p/n EAFLASH-128MB. [ more info]
For 6” C-more Panels (only)
Adapter Plate (6" EZ-Touch only)
If you are replacing an older 6" AutomationDirect EZTouch* with a C-more touch panel, you may need our adapter bezel. It's designed to allow C-more to fit the larger panel mounting hole that the old style 6" EZTouch required. If you are replacing a newer, or "slim bezel" EZTouch (Part numbers ending with "S") you will not need this adapter. [more info]