Automationdirect.com

AutomationDirect Offers Additional Fittings and Tubing

AutomationDirect Offers Additional Fittings and Tubing

Cumming, GA --- February 11, 2015 ... AutomationDirect's NITRA® line of pneumatics products now offers additional straight, branch, union, Y, reducer, elbow and bulkhead fittings in 1/8 inch and 5/16 inch tube connection sizes. Designed to work with flexible pneumatic tubing, select fittings are constructed with thermoplastic bodies and stainless steel tube gripping claws; additional fittings with nickel-plated brass bodies are also available.

NITRA inline fittings start at $5.25 for a five-pack and are backed by a one-year warranty.

Additional polyurethane tubing and nylon coiled hoses have also been added. Available in 100-foot packs ($13.50) and 500-foot reels ($67), 1/8-inch polyurethane tubing comes in seven colors, including UV-stabilized dark green making it an excellent choice for outdoor use.

Yellow nylon coiled hoses with nickel-plated brass male swivel NPT fittings are now offered in 1/4-inch, 3/8-inch and 1/2-inch sizes and in 10 to 40-foot lengths. Starting at $12.50, the heavy-duty nylon hoses have a low moisture absorption rate and are fitted with spring guards to resist kinking. Hose kits made up of 100-foot nylon hose and 10 replaceable fittings (enough material to make five hoses) are available starting at $63.00; individual replaceable fittings for repair of nylon hoses start at $11.

Learn more about NITRA pneumatic tubing and fittings by visiting: www.automationdirect.com/pneumatic-parts.

About AutomationDirect:
In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency and the majority of their products are stocked for same-day shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information, contact them at 800-633-0405 or visit www.automationdirect.com.

 

Editorial Contact:
TJ Johns
Phone: 678-455-1730
Email: tjohns@automationdirect.com


High resolution image: 300 dpi TIF (right click and Save Target As ...)