Automationdirect.com

AutomationDirect Adds Submersible Level Transmitters

AutomationDirect Adds Submersible Level Transmitters

Cumming, GA --- October 8, 2014 ... AutomationDirect's ProSense® line of level sensors now includes SLT series submersible level transmitters designed for applications such as lift station monitoring, construction by-pass pumping, tank liquid level, wastewater, and slurry tank liquid level control.

Available in two styles, the ProSense SLT series submersible level sensors provide liquid level measurement by continually sensing hydrostatic pressure produced by the height of liquid above the sensor and providing a 4-20 mA output signal compatible with PLCs, panel meters, data loggers, and other electronic equipment.

The SLT1 series features a slim 1-inch diameter housing and a ported bullet nose cap for protection of the sensor diaphragm. Starting at $299.00, this series is available in cable lengths ranging from 30 feet to 140 feet and with sensing ranges of 0-5 psig to 0-50 psig.

The SLT2 series features a large 2.75 inch diameter PTFE flexible diaphragm surrounded by a 316 stainless steel non-fouling protective cage to provide reliability and long life in harsh environments. Starting at $470.00, this series is available in cable lengths ranging from 30 feet to 100 feet and with sensing ranges of 0-5 psig to 0-30 psig.

Both styles are fitted with a shielded cable containing an atmospheric vent tube and a tough polyurethane jacket which incorporates an exclusive "water block" liner beneath the jacket. The cable is attached to the sensor using an over-molding process to prevent moisture intrusion.

Available accessories include a desiccant vent filter to prevent moisture from entering the vent tube and damaging transmitters with vented gage reference pressure; aneroid bellows which fluctuate with changes in atmospheric pressure to maintain a constant barometric reference; junction boxes to provide a water-resistant enclosure for electrically connecting the transmitter cable to the user's system via a terminal strip and replacement nose caps to protect the sensing diaphragm.

Made in the USA, all sensors are backed with a one-year warranty, include UL and FM hazardous location approvals for intrinsically safe applications and are CE marked.

To learn more and about the ProSense SLT series submersible level transmitters, visit: www.automationdirect.com/level-sensors.

About AutomationDirect:
In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor control, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their model and focus on efficiency and the majority of their products are stocked for same-day shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information, contact them at 800-633-0405 or visit www.automationdirect.com.

Editorial Contact:
TJ Johns
Phone: 678-455-1730
Email: tjohns@automationdirect.com


High resolution image: 300 dpi TIF (right click and Save Target As ...)