Automationdirect.com

AutomationDirect adds Air-to-Air Heat Exchangers for Enclosures

 AutomationDirect adds Air-to-Air Heat Exchangers for Enclosures

Cumming, GA --- September 18, 2013 ... AutomationDirect has expanded its Stratus™ line to include air-to-air heat exchangers in 120VAC and 24 VDC models. This air-to-air heat exchanger series is a closed-loop cooling system which employs the heat pipe principle to exchange heat from an electrical enclosure to the outside. Each heat pipe has an evaporator section and a condenser section which are separated by a permanent baffle so as to provide a closed loop. The coil systems use aluminum end plates and baffles which improve conduction and reduce corrosion for longer life.

Air-to-air heat exchanger prices start at $1,028.00 and are available in models for use with NEMA 4 and 4X enclosures. Units are offered in three frame sizes (compact, deep, and tall) up to 72 Watt capacity, and are equipped with two circulating fans with sealed overload protectors.

Air-to-air heat exchanger prices start at $1,028.00 and are available in models for use with NEMA 4 and 4X enclosures. Units are offered in three frame sizes (compact, deep, and tall) up to 72 Watt capacity, and are equipped with two circulating fans with sealed overload protectors. www.automationdirect.com/enclosure-heat-exchanger.

About AutomationDirect:
In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor control, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their model and focus on efficiency and the majority of their products are stocked for same-day shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information, contact them at 800-633-0405 or visit www.automationdirect.com.

 

Editorial Contact:
TJ Johns
Phone: 678-455-1730
Email: tjohns@automationdirect.com


High resolution image: 300 dpi TIF (right click and Save Target As ...)