The optional C-more AC Power Adapter can be used to power the C-more touch panels from a 100-240 VAC, 50/60 Hertz voltage source. The adapter provides 24 VDC @ 1.5 A to the touch panel's DC power connector and can be conveniently secured to the touch panel with two captive screws.
C-more accepts standard "off the shelf" SD Flash memory cards. SD Flash memory cards can be used to log alarms, messages, even PLC data. Capture the actual C-more screen when certain events occur, and store the screen image on the SD Flash card for later reference. If the C-more panel is on a network, the contents of the flash device can even be accessed via FTP or e-mailed from the panel, without removing the flash device from the panel.
Use SD cards to upload a project to a C-more panel without having a PC present. This feature is great for updating remotely located panels - just send a Compact Flash drive to any factory in the world, and remote C-more panels can be updated with the latest project.
AutomationDirect recommends and sells an SD Memory Card ( EA-SD-CARD ) an industrial-grade, high-speed memory card for non-volatile storage. One SD card can be installed in all C-more Panels. Up to 2 SD cards can be installed in the 12" and 15" C-more panels.
C-more accepts standard USB flash drives, sometimes called "pen drives". These small convenient drives are available in many sizes from less than 16 MB to more than 4GB of non-volatile memory.
USB drives can be used with C-more to log alarms, messages, even PLC data. Capture the actual C-more screen when certain events occur, and store the screen image on the USB drive for later reference. If the C-more panel is on a network, the contents of the USB drive can even be accessed via FTP or sent via e-mail (using the Event Manager) without removing it from the panel.
USB drives can also be used to upload a project to a C-more panel without having a PC present. This feature is great for updating remotely located panels - just send your project on a USB drive to any factory in the world, and remote C-more panels can be updated with the latest project.
AutomationDirect recommends and sells a 4GB SanDisk Cruzer Micro ( USB-FLASH) for use with the C-more Operator Touch Panels.
Use these screen protectors to protect your screens from harsh environments or harsh operators! Simply replace the protector periodically and "resurface" your panel. Sold in packages of three.
Part Numbers: EA-6-COV2, EA-7-COV2, EA-8-COV2, EA-10-COV2, EA-10W-COV2, EA-12-COV2 or EA-15-COV2
Equipment manufacturers will be pleased to see that the C-more panel can be "branded" with the manufacturer's own name or logo. The HMI is often a focal point for the machine, and now your logo can be front and center (well, in the upper, left corner anyway).
Blank label insert for front bezel, replacement, for C-more EA9 series touch panels. Package of 10.
Add More Ethernet to your panel for only $52.00 with the EA-ECOM module
The EA-ECOM module easily attaches to EA9 panels (excluding Base models) providing an additional 10/100 Base-T Ethernet Auto MDI/MDI-X RJ45 Port. Simply connect the module to the back of your EA9 C-more and secure it with the supplied screws. The EA-ECOM does not require an external power supply and supports all C-more Ethernet drivers.
Voted #1 mid-sized employer in Atlanta
Check out our
job openings