Hide Transcript
View Transcript
Turning a 3-phase motor on and off with a
PLC is easy enough. The PLC enables the contactor and the contactor
allows power to flow to the motor. While that does work, it’s not very realistic. In most practical applications there’s a
whole lot more to it. We’ll want to be able to monitor the status
of the branch circuit breaker and be able to trip the circuit breaker so we can shut
things down remotely and manage loads to make system startup easier. We need a button to turn the motor on and
we’ll want that to light up while it is running. We’ll need a way to stop the motor and let’s
have that button blink red for 5 seconds while the motor spins down and then turn solid red
when it is ok to re-start the motor. Of course we want to be able to monitor the
status of the overload and be able to test that it kills the power to the motor when
it trips. And finally, we want to be able to reverse
the motor and have all the necessary interlocks to ensure we don’t change the motor direction
while it is powered. And of course, we’ll want surge suppression
on the contactors to protect our controller from the voltage spikes. That’s a little more involved than just
turning a motor on and off, but it really isn’t that bad. In this video we’ll review how all of this
gets wired together and then in the next video we’ll program an Automation Direct Do-More
Controller to monitor and control this reversing A/C Motor on off system. At first glance the wiring looks intimidating,
but if we take it one step at a time … it really isn’t that bad. Our controller has an input module with 16
inputs and an output module with 4 relay outputs. And we want to use those to control and monitor
a 3-phase motor on a branch circuit. We’ll start with the circuit breaker that
provides us the 3-phase power. We want to be able to monitor the status of
the breaker so we add an aux contact to the circuit breaker and bring that into input
X0. While we could use either the normally open
or normally closed contact here, we prefer to use a normally open contact so loose or
broken wires will be detected while the circuit breaker is powered up. This serves as a failsafe for our circuit
and is a good habit to get into. We want to be able to trip this breaker remotely,
so let’s add a shunt trip which we will drive from output Y0. We can now monitor and control the branch
circuit breaker – check that off the list. Next we add a contactor – we’re using
a WEG mini contactor in this demo because they are so easy and convenient to use. And they’re very capable - they can handle
up to 25 amps. We’ll control it from output Y1 and we’ll
call that the Forward Direction. We definitely want surge protection, which
for this contactor is just a plug in module, and we want to monitor the status of the contactor
so we’ll add an aux contact module with a normally open contact going into input X1. Could we have used this built in aux contact
that the WEG contactor has for this? Sure, but we chose this particular contactor
with the normally closed built-in contact because it will make adding reversing easier
when we get to that step, so we’ll leave that one alone for now and use the aux contact
module to monitor the status of the contactor. Finally, we’ll need an overload protector
and we’ll have the overload reported on closure of the overloads normally open aux
contact into input X3 on the controller. Remember – the overload doesn’t kill the
power – it just reports that there is an issue. So we’ll use the overloads normally closed
contact to kill the power to the contactors coil. We want to use the normally closed contact
for this because it is connected when the overload isn’t tripped, but also because
if there is a loose connection or a broken wire it will also keep the motor from running. If we used the normally open contact to somehow
interrupt the contactors coil, we wouldn’t be able to detect any wiring faults. So use of the normally closed contact helps
make the system “fail safe.” Well, that’s all we need to control a motor
in one direction. That wasn’t so bad …
We can monitor and control the Branch Circuit Breaker, We can enable the contactor, monitor
the contactor, protect the PLC from surges, protect our motor against overload and monitor
the status of the overload. Perfect. To add reversing, we just add a second contactor
and do two more things to the wiring. First, if the motor is powered through this
contactor and rotating in the forward direction, we don’t want the reverse contactor to engage,
that would short out the wiring and bad things would happen. And likewise, if the motor is going in reverse,
we don’t want the forward contactor to engage. To fix that we modify the control wiring a
little bit. Instead of controlling the forward contactor
directly, we run the control wire through the aux contact on the revering contactor. So if the reversing contactor is engaged,
there is no way the forward contactor be turned on. We do the same thing for the reverse contactor
– run his control wire through the forward contactor’s aux contact. So if the FORWARD contactor is engaged, there
is no way the REVERSE contactor can be turned on. And finally we need to run a copy of the power
lines through the second contactor taking care to cross one set of wires to get the
reversing action. The good news is this wiring is already done
for you in these reversing kits – just plug them in. Some reversing kits require YOU to do the
fail safe wiring yourself. With these WEG contactors we are using, all
you need to do is run the one wire to each normally closed contact and the single neutral
– the fail safe wiring is all built into the bus bars. We also want to monitor the status of the
reverse contactor so we’ll add another aux contact to that guy and run that into input
X2 and we’ll want to add surge suppression to the reversing contactor too. We’ll also add a mechanical interlock. We already made sure that one contactor can’t
engage when the other is active by wiring the coils through the other contactors aux
contact. This mechanical interlock does the same thing. When one contactor is engaged, it physically
prevents the other contactors armature from moving – same function as the wiring, but
this time it is purely mechanical. It adds an extra layer of protection. And having both electrical AND mechanical
interlocks is required by some codes. And there you have it. A full reversing AC motor start stop control
circuit with the ability to remotely trip and monitor the breaker, remotely monitor
the overload, electrical and mechanical fail-safes built in to protect us from wiring shorts
if the controller accidentally tries to engage both contactors at the same time and over
load protection. Keep in mind that while we didn’t show it
in this simple wiring diagram, proper grounding and wiring in accordance with the national
and local electrical codes is assumed. Here’s a photo of the test rack and all
of the parts used in this video. There’s a lot of extra wires and connectors
on this guy so we can swap out controller and subject matter panels for other videos,
but functionally, it’s identical to the wiring diagrams we created in this how to
video. Join us in Part II of this video where we
will write the PLC code to control and manage all of this. If you need more details on any of the items
we are using here, check out the companion Tech Tip videos – they go into great detail
on every one of these items. If you have any questions about any of this,
please don’t hesitate to call Automation Directs free award winning tech support during
regular business hours – they will be happy to help you. And check out the forums – there are lots
of folks there that love to share their years of experience – just don’t ask and support
questions there – they don’t monitor the forms on a regular basis
Draft comments (Joe Kimbrell)