What is an IEC Gearbox? from AutomationDirect


Related Products

WGA-63M-020-90B5
WGA-63M-020-90B5 Thumbnail
18I1
18I1 Thumbnail
18HZ
18HZ Thumbnail
18I6
18I6 Thumbnail
14JQ
14JQ Thumbnail
18I8
18I8 Thumbnail
8IA
8IA Thumbnail
13HB
13HB Thumbnail
18IC
18IC Thumbnail
18Q3
18Q3 Thumbnail
18Q4
18Q4 Thumbnail
18Q5
18Q5 Thumbnail
18Q6
18Q6 Thumbnail
18Q7
18Q7 Thumbnail
18IY
18IY Thumbnail
18OM
18OM Thumbnail
18ON
18ON Thumbnail
18J4
18J4 Thumbnail
0NX5
0NX5 Thumbnail
0NX7
0NX7 Thumbnail
0NXA
0NXA Thumbnail
0VNF
0VNF Thumbnail
0UQR
0UQR Thumbnail
0NUL
0NUL Thumbnail
0NUN
0NUN Thumbnail
0NUP
0NUP Thumbnail
0RC2
0RC2 Thumbnail
16SV
16SV Thumbnail
131C
131C Thumbnail
WGA-63M-030-80B14
WGA-63M-030-80B14 Thumbnail
WGA-63M-030-80B5
WGA-63M-030-80B5 Thumbnail
WGA-63M-030-90B14
WGA-63M-030-90B14 Thumbnail
WGA-63M-030-90B5
WGA-63M-030-90B5 Thumbnail
WGA-63M-040-71B14
WGA-63M-040-71B14 Thumbnail
WGA-63M-040-71B5
WGA-63M-040-71B5 Thumbnail
WGA-63M-040-80B14
WGA-63M-040-80B14 Thumbnail
WGA-63M-040-80B5
WGA-63M-040-80B5 Thumbnail
WGA-63M-050-71B14
WGA-63M-050-71B14 Thumbnail
WGA-63M-050-71B5
WGA-63M-050-71B5 Thumbnail
WGA-63M-050-80B14
WGA-63M-050-80B14 Thumbnail
WGA-63M-050-80B5
WGA-63M-050-80B5 Thumbnail
WGA-63M-060-71B14
WGA-63M-060-71B14 Thumbnail
WGA-63M-060-71B5
WGA-63M-060-71B5 Thumbnail
WGA-63M-060-80B14
WGA-63M-060-80B14 Thumbnail
WGA-63M-060-80B5
WGA-63M-060-80B5 Thumbnail
WGA-63M-080-71B14
WGA-63M-080-71B14 Thumbnail
WGA-63M-080-71B5
WGA-63M-080-71B5 Thumbnail
WGA-63M-080-80B14
WGA-63M-080-80B14 Thumbnail
WGA-63M-080-80B5
WGA-63M-080-80B5 Thumbnail
WGA-75M-100-80B14
WGA-75M-100-80B14 Thumbnail
WGA-75M-100-80B5
WGA-75M-100-80B5 Thumbnail
WGA-75M-020-80B14
WGA-75M-020-80B14 Thumbnail
WGA-75M-020-80B5
WGA-75M-020-80B5 Thumbnail
WGA-75M-020-90B14
WGA-75M-020-90B14 Thumbnail
WGA-75M-020-90B5
WGA-75M-020-90B5 Thumbnail
WGA-75M-030-80B14
WGA-75M-030-80B14 Thumbnail
WGA-75M-030-80B5
WGA-75M-030-80B5 Thumbnail
WGA-75M-030-90B14
WGA-75M-030-90B14 Thumbnail
WGA-75M-030-90B5
WGA-75M-030-90B5 Thumbnail
WGA-75M-040-80B14
WGA-75M-040-80B14 Thumbnail
WGA-75M-040-80B5
WGA-75M-040-80B5 Thumbnail
WGA-75M-040-90B14
WGA-75M-040-90B14 Thumbnail
WGA-75M-040-90B5
WGA-75M-040-90B5 Thumbnail
WGA-75M-050-80B14
WGA-75M-050-80B14 Thumbnail
WGA-75M-050-80B5
WGA-75M-050-80B5 Thumbnail
WGA-75M-060-80B14
WGA-75M-060-80B14 Thumbnail
WGA-75M-060-80B5
WGA-75M-060-80B5 Thumbnail
WGA-75M-080-80B14
WGA-75M-080-80B14 Thumbnail
WGA-75M-080-80B5
WGA-75M-080-80B5 Thumbnail
WGA-30M-S-IEC
WGA-30M-S-IEC Thumbnail
WGA-40M-S-IEC
WGA-40M-S-IEC Thumbnail
WGA-50M-S-IEC
WGA-50M-S-IEC Thumbnail
WGA-63M-S-IEC
WGA-63M-S-IEC Thumbnail
WGA-75M-S-IEC
WGA-75M-S-IEC Thumbnail
WGA-30M-D-IEC
WGA-30M-D-IEC Thumbnail
WGA-40M-D-IEC
WGA-40M-D-IEC Thumbnail
WGA-50M-D-IEC
WGA-50M-D-IEC Thumbnail
WGA-63M-D-IEC
WGA-63M-D-IEC Thumbnail
WGA-75M-D-IEC
WGA-75M-D-IEC Thumbnail
WGA-50M-050-71B5
WGA-50M-050-71B5 Thumbnail
WGA-50M-060-71B14
WGA-50M-060-71B14 Thumbnail
WGA-50M-060-71B5
WGA-50M-060-71B5 Thumbnail
WGA-50M-080-71B14
WGA-50M-080-71B14 Thumbnail
WGA-50M-080-71B5
WGA-50M-080-71B5 Thumbnail
WGA-63M-010-80B14
WGA-63M-010-80B14 Thumbnail
WGA-63M-010-80B5
WGA-63M-010-80B5 Thumbnail
WGA-63M-010-90B14
WGA-63M-010-90B14 Thumbnail
WGA-63M-010-90B5
WGA-63M-010-90B5 Thumbnail
WGA-63M-100-71B14
WGA-63M-100-71B14 Thumbnail
WGA-63M-100-71B5
WGA-63M-100-71B5 Thumbnail
WGA-63M-100-80B14
WGA-63M-100-80B14 Thumbnail
WGA-63M-100-80B5
WGA-63M-100-80B5 Thumbnail
WGA-63M-020-80B14
WGA-63M-020-80B14 Thumbnail
WGA-63M-020-80B5
WGA-63M-020-80B5 Thumbnail
WGA-63M-020-90B14
WGA-63M-020-90B14 Thumbnail
0YGA
0YGA Thumbnail
0YGB
0YGB Thumbnail
0ZYZ
0ZYZ Thumbnail
18J7
18J7 Thumbnail
18PU
18PU Thumbnail
18J8
18J8 Thumbnail
18OR
18OR Thumbnail
18J9
18J9 Thumbnail
18PL
18PL Thumbnail
18OT
18OT Thumbnail
WGA-30M-010-63B14
WGA-30M-010-63B14 Thumbnail
WGA-30M-010-63B5
WGA-30M-010-63B5 Thumbnail
WGA-30M-020-63B14
WGA-30M-020-63B14 Thumbnail
WGA-30M-020-63B5
WGA-30M-020-63B5 Thumbnail
WGA-30M-030-63B14
WGA-30M-030-63B14 Thumbnail
WGA-30M-030-63B5
WGA-30M-030-63B5 Thumbnail
WGA-30M-040-63B14
WGA-30M-040-63B14 Thumbnail
WGA-30M-040-63B5
WGA-30M-040-63B5 Thumbnail
WGA-30M-050-63B14
WGA-30M-050-63B14 Thumbnail
WGA-30M-050-63B5
WGA-30M-050-63B5 Thumbnail
WGA-40M-010-63B14
WGA-40M-010-63B14 Thumbnail
WGA-40M-010-63B5
WGA-40M-010-63B5 Thumbnail
WGA-40M-010-71B14
WGA-40M-010-71B14 Thumbnail
WGA-40M-010-71B5
WGA-40M-010-71B5 Thumbnail
WGA-40M-100-63B14
WGA-40M-100-63B14 Thumbnail
WGA-40M-100-63B5
WGA-40M-100-63B5 Thumbnail
WGA-40M-020-63B14
WGA-40M-020-63B14 Thumbnail
WGA-40M-020-63B5
WGA-40M-020-63B5 Thumbnail
WGA-40M-020-71B14
WGA-40M-020-71B14 Thumbnail
WGA-40M-020-71B5
WGA-40M-020-71B5 Thumbnail
WGA-40M-030-63B14
WGA-40M-030-63B14 Thumbnail
WGA-40M-030-63B5
WGA-40M-030-63B5 Thumbnail
WGA-40M-030-71B14
WGA-40M-030-71B14 Thumbnail
WGA-40M-030-71B5
WGA-40M-030-71B5 Thumbnail
WGA-40M-040-71B14
WGA-40M-040-71B14 Thumbnail
WGA-40M-040-71B5
WGA-40M-040-71B5 Thumbnail
WGA-40M-050-63B14
WGA-40M-050-63B14 Thumbnail
WGA-40M-050-63B5
WGA-40M-050-63B5 Thumbnail
WGA-40M-060-63B14
WGA-40M-060-63B14 Thumbnail
WGA-40M-060-63B5
WGA-40M-060-63B5 Thumbnail
WGA-40M-080-63B14
WGA-40M-080-63B14 Thumbnail
WGA-40M-080-63B5
WGA-40M-080-63B5 Thumbnail
WGA-50M-010-71B14
WGA-50M-010-71B14 Thumbnail
WGA-50M-010-71B5
WGA-50M-010-71B5 Thumbnail
WGA-50M-010-80B14
WGA-50M-010-80B14 Thumbnail
WGA-50M-010-80B5
WGA-50M-010-80B5 Thumbnail
WGA-50M-020-71B14
WGA-50M-020-71B14 Thumbnail
WGA-50M-020-71B5
WGA-50M-020-71B5 Thumbnail
WGA-50M-020-80B14
WGA-50M-020-80B14 Thumbnail
WGA-50M-020-80B5
WGA-50M-020-80B5 Thumbnail
WGA-50M-030-71B14
WGA-50M-030-71B14 Thumbnail
WGA-50M-030-71B5
WGA-50M-030-71B5 Thumbnail
WGA-50M-030-80B14
WGA-50M-030-80B14 Thumbnail
WGA-50M-030-80B5
WGA-50M-030-80B5 Thumbnail
WGA-50M-040-71B14
WGA-50M-040-71B14 Thumbnail
WGA-50M-040-71B5
WGA-50M-040-71B5 Thumbnail
WGA-50M-050-71B14
WGA-50M-050-71B14 Thumbnail


Visit www.AutomationDirect.com for products and prices. (VID-PT-0021)


Hide Transcript
View Transcript

Automation Direct sells both IEC motors and gearboxes for many applications. Many of us in the North American market may be more familiar with NEMA motors, which are sized based on imperial or SAE measurements such as inches. IEC motors use metric measurements such as millimeters. In here, I'll look at the differences with IEC motors. On IEC motors, the frame size is very similar to a NEMA frame size, which tells us the height of the shaft, shaft diameter, and mounting dimensions in millimeters. The second component of IEC motor specifications is the mounting designation, much like a C-face on a NEMA motor. This tells us the mounting options such as B14 which designates a C-face, or B5, is a D-face. When selecting compatible devices, ratings and mechanical fit need to be considered. So, a NEMA 56C motor will fit a gearbox with a 56C input flange, and IEC 63B14 motor will fit a gearbox with a 63B14 input flange. But you must ensure the gearbox is matched by rating, such as gearbox input power should not be exceeded by the motor. A quick note, if you’re not familiar, gearboxes, also known as enclosed gear drives or speed reducers, are mechanical drive components that reduce the drive's speed as well as increase the motor’s torque by the gear ratio. For example, with a 10:1 ratio, the gearbox output is 1/10th of the motor speed and 10 times the motor's torque at approximately the same motor output horsepower minus losses. IronHorse IEC worm gearboxes contain a worm on the input shaft and a mating gear on the output shaft, which is arranged at 90 degrees to the input shaft. The cast aluminum housing offers lightweight design and optimal heat dissipation. We offer single- and double-output shafts, output flanges, torque arms, and output covers. AutomationDirect is the number one value in Automation.



No data returned!
An error has occurred! Please contact support
Videos Home > What is an IEC Gearbox? from AutomationDirect