Filter Results Clear All
You've selected:
> Programmable Controllers > BRX PLCs (Stackable Micro Brick)
  •   Shop  
  •   Overview  
  •   In Depth  
BRX Home BRX - Your Automation Foundation Configure a BRX
 
Features
10 ways it's better with BRX PLCs! Communication Options IIoT Edge Device - Your low cost link to Industry 4.0Integrated Motion on Multiple Levels Not Your Everyday Analog Security Simple Data Logging/Advanced Data Control Fortified with American Pride Easy Migration Motion Control/Positioning made easy! BRX IIoT in Motion
Free Software
What's New with Do-more Designer Dashboard - Easy Navigation Simulator IIoT WebServer Connectivity Motion on Multiple Levels Simple Data Logging Data Delivered Easy PID Video Help Auto-Discover I/O Powerful Math Trouble free Troubleshooting DirectLOGIC Migration Free Online Training Download the Free Software
Hardware
Hardware Overview M Series CPUs (no I/O) 10-point Series CPUs 18-point Series CPUs 36-point Series CPUs Ethernet Remote I/O Expansion Modules Pluggable Option Modules Connection Options Spare Parts Go to ZIPLink Selector Tool
Instruction Set
Videos


BRX Series PLCs (Stackable Micro Brick): Do-more Designer Videos

Detailed Product
Overview



To learn more: https://www.automationdirect.com/do-more?utm_source=t6VUBRZUQ0w&utm_medium=VideoTeamDescription - (VID-DD-0054)

This video gives basic information on Using the Stage instruction in the Do-more Designer software. It presents information that is commonly missed by users.
** Software Version used in this video: Do-more Designer 2.0.3

Online Support Page: https://community.automationdirect.com/s/?utm_source=t6VUBRZUQ0w&utm_medium=VideoTeamDescription

**Please check our website for our most up-to-date product pricing and availability.


Hide Transcript
View Transcript
This instruction marks the beginning of a

stage, and stages can only be entered in Program code blocks. Each Program code block can have up to 128

stages and there cannot be duplicates stages, within the same code block. This is a 'power-rail' instruction. This just means that even though it is displayed

on the left hand side of the logic, it is actually entered in on the right-hand side

of the logic and then collapses down to the Power rail. The first Stage instruction in a Program code

block, regardless of the stage number, will automatically become the "Initial Stage",

and this will be indicated, as the initial stage, because it will have a double border. Whenever a Program code block is first enabled

to run, the Initial Stage will automatically be enabled and all of the other stages will

be disabled. After the first scan of the Program code block

the Initial Stage will operate like any other stage in the Program code block.


BRX Do-more PLCs Do-more Designer Software & Programming
  • Video
    BRX Do-more Designer Using the CALL Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the ENDC Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the ENTASK Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the EXIT Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the GOTO Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the HALT Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the LABEL Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the REBOOT Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the RESTART Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the RET Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the RETC Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the INTCONFIG Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the INTDECONFIG Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the INTRESUME Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the INTSUSPEND Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the JMP Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the JMPI Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the RUN Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the STOP Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the SUSPEND Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the WATCHDOG Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the YIELD Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the SG Stage Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the SGCONVRG Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the SGDIVRG Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the SGRST Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the SGRSTR Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the SGSET Instruction from AutomationDirect

Playlist Not Found Could not find playlist PLPdypWXY_ROovolXmvgjO63qk2RdsoIGx

Playlist Not Found Could not find playlist PLPdypWXY_ROoIDZ7MO4OLz8AMJ_lExObe

Playlist Not Found Could not find playlist PLPdypWXY_ROoiFQetOa9Kc_9NF3dLgQon