Hide Transcript
View Transcript
This instruction is used to stop the processing
of a configured interrupt trigger. This instruction can only be used with a BRX
style CPU, and will not work with the H2 or T1H series Do more CPUS. An interrupt can be configured using the Interrupt
config instruction or from the system configuration and this instruction will stop the processing
of both of these types, but it cannot permanently delete the interrupt configuration from the
system configuration. So, if the trigger was created from the system
config and there is a Program to Run transition, it will reload that found in the system configuration.