Hide Transcript
View Transcript
This instruction should only be used, to write
to a Directlogic PLC. If you are using an ECOM or ecom100, as your
master device, Slave ID is the only option you will have available. You will need to use Netedit tool to set up
this ID. When using the internal Ethernet port, all
three addressing options are available, but I find it best to use Fixed or variable addressing. This is the most common stumbling block, notice
this instruction uses number of bytes and not number of addresses. These are the ways that this instruction can
be triggered. I usually set the instruction for the following
settings with a constant time of 1 second until I can verify I have good Communications. For more information on this instruction click
here