• Credit Application
  • Tax Exemption
| Direct Sales in US and Canada | 1-800-633-0405 | About Us | Contact Us | Line Card
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
Ironhorse ACN & ACG VFD Modbus TCP Setup from AutomationDirect


Related Products

ACNND-23P0
ACNND-23P0 Thumbnail
ACNND-25P0
ACNND-25P0 Thumbnail
ACNND-27P5
ACNND-27P5 Thumbnail
ACNND-2010
ACNND-2010 Thumbnail
ACNND-2015
ACNND-2015 Thumbnail
ACNND-2020
ACNND-2020 Thumbnail
ACNND-40P5
ACNND-40P5 Thumbnail
ACNND-41P0
ACNND-41P0 Thumbnail
ACNND-42P0
ACNND-42P0 Thumbnail
ACNND-43P0
ACNND-43P0 Thumbnail
ACNND-45P0
ACNND-45P0 Thumbnail
ACNND-47P5
ACNND-47P5 Thumbnail
ACNND-4010
ACNND-4010 Thumbnail
ACNND-4015
ACNND-4015 Thumbnail
ACNND-4020
ACNND-4020 Thumbnail
ACNND-4025
ACNND-4025 Thumbnail
ACNND-4030
ACNND-4030 Thumbnail
ACG-ET2
ACG-ET2 Thumbnail
ACN-ETH
ACN-ETH Thumbnail
ACG-20P5
ACG-20P5 Thumbnail
ACG-21P0
ACG-21P0 Thumbnail
ACG-22P0
ACG-22P0 Thumbnail
ACG-23P0
ACG-23P0 Thumbnail
ACG-25P0
ACG-25P0 Thumbnail
ACG-27P5
ACG-27P5 Thumbnail
ACG-2010
ACG-2010 Thumbnail
ACG-2015
ACG-2015 Thumbnail
ACG-2020
ACG-2020 Thumbnail
ACG-40P5
ACG-40P5 Thumbnail
ACG-41P0
ACG-41P0 Thumbnail
ACG-42P0
ACG-42P0 Thumbnail
ACG-43P0
ACG-43P0 Thumbnail
ACG-45P0
ACG-45P0 Thumbnail
ACG-47P5
ACG-47P5 Thumbnail
ACG-4010
ACG-4010 Thumbnail
ACG-4015
ACG-4015 Thumbnail
ACG-4020
ACG-4020 Thumbnail
ACG-4025
ACG-4025 Thumbnail
ACG-4030
ACG-4030 Thumbnail
ACN-2010
ACN-2010 Thumbnail
ACN-2015
ACN-2015 Thumbnail
ACN-2020
ACN-2020 Thumbnail
ACN-40P5
ACN-40P5 Thumbnail
ACN-41P0
ACN-41P0 Thumbnail
ACN-42P0
ACN-42P0 Thumbnail
ACN-43P0
ACN-43P0 Thumbnail
ACN-45P0
ACN-45P0 Thumbnail
ACN-47P5
ACN-47P5 Thumbnail
ACN-4010
ACN-4010 Thumbnail
ACN-4015
ACN-4015 Thumbnail
ACN-4020
ACN-4020 Thumbnail
ACN-4025
ACN-4025 Thumbnail
ACN-4030
ACN-4030 Thumbnail
ACNND-20P5
ACNND-20P5 Thumbnail
ACNND-21P0
ACNND-21P0 Thumbnail
ACNND-22P0
ACNND-22P0 Thumbnail
ACN-20P5
ACN-20P5 Thumbnail
ACN-21P0
ACN-21P0 Thumbnail
ACN-22P0
ACN-22P0 Thumbnail
ACN-23P0
ACN-23P0 Thumbnail
ACN-25P0
ACN-25P0 Thumbnail
ACN-27P5
ACN-27P5 Thumbnail


To learn more: https://www.automationdirect.com/ac-drives?utm_source=CdjIotS1kMI&utm_medium=VideoTeamDescription

(VID-DR-0387)

Learn how to set up Ironhorse ACN and ACG series variable frequency drives (VFDs) for Modbus TCP communication.

Related videos:
• Modbus RTU Series (Part 1 & 2) – https://www.youtube.com/watch?v=WnUOm21lYrk


https://youtu.be/eLRJ92S4Xio
• Ironhorse Drive Basics and Motor Parameter Setup

https://youtu.be/tGhUkALA24s

https://community.automationdirect.com/s/contactsupport?utm_source=CdjIotS1kMI&utm_medium=VideoTeamDescription

**Please check our website for our most up-to-date product pricing and availability.


Hide Transcript
View Transcript

We’re setting up two Ironhorse VFDs for Modbus TCP communication. One ACN series and one ACG series. The setup is almost the same, but I’ll point out any differences along the way. Of course, first we need to install the modules. On the ACG, it’s simple. Remove this cover, connect the short cable between the drive and the card. Snap the module in to place, and tighten the screw. The card has two Ethernet ports for daisy-chaining drives, plus a covered connector for a PC or remote keypad. Just pop out the cover if you need to use it. On the ACN, the installation takes a few extra steps, but it’s still pretty straightforward. The option card also has a covered RS-485 port, so make sure you use the proper port for Ethernet. Before installing, switch one up for Modbus TCP. Remove the drive front cover and the module cover. Disconnect this wiring connector. Remove the keypad adapter board. Then, install the extenders. The short one goes on the right, and remove the screw on the left to install the longer one. Now, snap in the card, secure it with the screw that came with the card, and the one you just removed. Reinstall the keypad adapter board. Reconnect the wiring, and snap the ETH cover back in place. When the cards are powered, the CPU LED should flash, confirming it’s communicating with the drive. If it’s not flashing, please reinstall the card. Now let’s set up our drives. We’ll assume you’ve already set the motor parameters. If not, please see the video linked above. Now let’s set the drive control to the network. On the keypad, use the up arrow to get to DRV and set it to 4 for Fieldbus. Then go to FRQ, and set it to 8 for Fieldbus. Next, assign network settings. The IP address is in parameters CM10 through 13 Subnet mask is in CM14 through 17, and Gateway is in CM18 through 21. I’ve checked the PLC program, and it uses 192.168.1.101 and 192.168.1.31. Since dot 101 is the default for the ACG, we’ll leave it. For the ACN, we’ll set it to 192.168.1.31. And use the default for mask and gateway on both. And to retain these settings through a power cycle, they must be stored by setting CM94 to 1. I didn’t bother with this step on the ACG since it’s all default. That’s the basic setup. But our PLC program also uses the virtual inputs, so let’s configure those too. So, set CM70 for virtual DI1 to 46 for forward jog, and CM71 for virtual DI2 to 47 for reverse jog. We have a two-part Modbus RTU series linked in the description, and above, please see that if you’d like a closer look at Modbus. TCP works mostly the same, but keep in mind, the addresses are offset by one. For example, the status word is 40773 in RTU, but 40774 in TCP. All the Modbus addresses can be found in chapter 5 of the drives’ user manual. Now for the PLC program. If you’re using one of our PLCs, we provide example programs for every drive and PLC. Here, I’m using a CLICK PLC and a C-more HMI for interfacing. The CLICK data view makes it easy to manipulate values, but I felt like making a C-more project for this. The CLICK program is well-documented. We set the number of drives here; this controls message stepping. If you need more than 2 drives, you’ll need to add more messages. The program calculates RPM from the frequency command. Error and success counters help monitor communication. Bits for start/stop and direction are packed into word DS1103. So, the messaging flow goes like this: First, we read from Drive 1: 8 words starting at 40785, which include output current, frequency, RPM. With the drive being stopped, we only see bus voltage right now. Next, we write the frequency command from DS1101, along with RPM and operation bits. The drive runs at 30 Hz, and we see the expected feedback. Drive 2’s messaging is exactly the same. So we tell Drive 2 to run at 60 Hz. And again, we get the feedback we expect. Finally, lets test the jog with the virtual D'is. And that also works as expected. That’s it! Two Ironhorse VFDs running over Modbus TCP. For more drive videos, look here. To buy drives for your applications, click here, and subscribe to be notified of new products and solutions.



No data returned!
An error has occurred! Please contact support
Videos Home > Ironhorse ACN & ACG VFD Modbus TCP Setup from AutomationDirect
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
Copyright © 1999-2025 AutomationDirect.  ALL RIGHTS RESERVED.
Site Map     Send Us your Feedback     Unsubscribe     Email Preferences     Legal & Business Policies     YouTube Terms of Service
Clear login credentials



Back to Top


spinner Updating...
Info