AutomationDirect
Login | Register
Accounts & Orders
Cart
3
$221.00

Recent Orders

View and Manage | Request Cancellation
Loading Order History
Loading...

Your Account

Account Home

Checkout   $221.00
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
Videos Home > WEG CFW500 VFD PID Quick Start...

WEG CFW500 VFD PID Quick Start 2 from AutomationDirect


Related Products

15570800
15570800 Thumbnail
15571879
15571879 Thumbnail
15571881
15571881 Thumbnail
15574655
15574655 Thumbnail
15575067
15575067 Thumbnail
15572625
15572625 Thumbnail
15572689
15572689 Thumbnail
15575202
15575202 Thumbnail
15575701
15575701 Thumbnail
15575716
15575716 Thumbnail
15576540
15576540 Thumbnail
15577077
15577077 Thumbnail
15342437
15342437 Thumbnail
15342760
15342760 Thumbnail
15342909
15342909 Thumbnail
15572819
15572819 Thumbnail
15572908
15572908 Thumbnail
15573714
15573714 Thumbnail
15573819
15573819 Thumbnail
15573823
15573823 Thumbnail
15575568
15575568 Thumbnail
15575577
15575577 Thumbnail
15575665
15575665 Thumbnail
15575699
15575699 Thumbnail
15575707
15575707 Thumbnail
15576919
15576919 Thumbnail
15577021
15577021 Thumbnail
15577211
15577211 Thumbnail
15577452
15577452 Thumbnail
15733937
15733937 Thumbnail
15734064
15734064 Thumbnail
15734119
15734119 Thumbnail
14990863
14990863 Thumbnail
14991103
14991103 Thumbnail
14991753
14991753 Thumbnail
14938005
14938005 Thumbnail
14938047
14938047 Thumbnail
14938113
14938113 Thumbnail
14975838
14975838 Thumbnail
14938655
14938655 Thumbnail
14991953
14991953 Thumbnail
14992148
14992148 Thumbnail
14976517
14976517 Thumbnail
14976809
14976809 Thumbnail
14977065
14977065 Thumbnail
14977266
14977266 Thumbnail
14977397
14977397 Thumbnail
14978365
14978365 Thumbnail
14978573
14978573 Thumbnail
14989840
14989840 Thumbnail
14990985
14990985 Thumbnail
14991517
14991517 Thumbnail
14937890
14937890 Thumbnail
14938041
14938041 Thumbnail
14938111
14938111 Thumbnail
14975783
14975783 Thumbnail
14938547
14938547 Thumbnail
14991899
14991899 Thumbnail
14992113
14992113 Thumbnail
14975888
14975888 Thumbnail
14976683
14976683 Thumbnail
14976814
14976814 Thumbnail
14977261
14977261 Thumbnail
14977391
14977391 Thumbnail
14977629
14977629 Thumbnail
14978548
14978548 Thumbnail


To learn more: https://www.AutomationDirect.com/drives?utm_source=NYMhFaTCMFQ&utm_medium=VideoTeamDescription

(VID-DR-0326)

In Part 1 we learned about our hardware. Given that we are ready to configure all the parameters. This video will show you a super simple way to get it right every time and in a matter of minutes we'll have our System automatically maintaining pressure using the drives built-in PID. The WEG CFW500 drive also has an "Internal PID" that runs in the Soft PLC built-in to the drive.

PID Support Files And Configuration Tools: https://cdn.automationdirect.com/static/video-resources/drives/WEG_CFW500/CFW500-PID-Support-Files.zip

Online Support Page: https://community.automationdirect.com/s/?utm_source=NYMhFaTCMFQ&utm_medium=VideoTeamDescription

**Please check our website for our most up-to-date product pricing and availability.


Hide Transcript
View Transcript

In Part 1, we found out that our system is capable of holding 6 psi regardless of how many valves we have opened, that we had plenty of extra motor speed to help PID accelerate quickly, and which motor speeds correspond to the min and max sensor readings. Now we just enter the PID-related parameters and turn it on – right? Well, in theory - yes. But there are a lot of parameters to keep track of which can make PID seem overwhelming. The good news is, I’ve sifted through all the related parameters and pulled out the bare minimum you’ll need to get up and running quickly, and arranged them into an excel spreadsheet configuration tool that looks like this. It’s just your basic feedback diagram where we take the set point and the process variable, take the difference to produce an error signal, run that through the PID algorithm, and send the control output to the motor. The parameters associated with each of those are grouped around each item plus the motor control group, the drive control group, and the display configuration parameters. This legend tells you what the colors mean. All of the blue parameters are factory defaults and the gray cells are read-only, so all we have to do is take one group at a time and fill in the yellow blanks. When we do those turn white. Before we get started please note that this worksheet applies only to the WEG CFW500 drive’s built-in PID. It doesn’t apply to the internal or external PLC application versions of PID that the CFW500 also has. We’ll do a separate version for those. And this is a summary of how this system is set up. I’m using this drive exactly as we left it in Part 1 where we had done a factory reset so you know exactly where I am starting from, we entered the motor parameters you see here in white and the display parameters shown in white. Let’s enter the min and max drive frequency parameters we found in the previous video just to finish that section. Great, all the yellow cells are gone so that section is done. When you press the up-down arrow keys on the keypad the result gets converted to engineering units and stored here. It’s gray to remind us it is read only. This is the value we want to show on the display. The raw set point is in percent and is stored in Parameter 525. We want 6 psi, which is 40% of our sensor's 15 psi range, so we put a 40 here. The filter is for when you use an analog input for your set point. We’re entering the set point from the HMI keypad, so filtering doesn’t matter. We’ll leave it at the blue default value. If you see a little red triangle in the cell, then there is a hover note explaining what I did or listing relevant options. For most applications, you will find that these blue default PID coefficients will be a great starting point – especially for monitoring pressure in pumping applications. The manual has this awesome chart that gives you good values to start with for other types of applications like flow, temperature, etc., so I highly recommend starting with the values in this table. If you want to tweak those, check out this video that shows you how to tune a PID loop on a CFW300 drive. The techniques shown in that video apply exactly the same way to the CFW500 drive. Let’s set up the drive control. To keep things simple, we are going to set this drive up for remote mode only. That way we don’t have to remember to make sure we are in the right mode. Again the little red triangle reminds us there is a note that has all the relevant options listed out. Looks like we want a 1 for remote only so I’ll enter that here. We’ll use the HMI for the speed reference or set point. The drive defaults to having a digital input control run stop in remote mode, so we’ll keep that blue default value too. Digital Input 1 is the default for run stop in remote mode so that’s good too. And we’ll use Digital Input 2 to control the manual auto operation of the PID loop, which is a 22. That means Digital Input 2 controls this guy. When we flip that switch to Auto, the PID loop runs normally. When we flip him to Manual, it stops the PID process and allows us to manually enter whatever value we want to appear at the control output. We enter that value in Parameter 121 in Hertz. We’ll set that to zero so we don’t get any surprises when we turn this thing on. Bumpless mode prevents large changes or large “bumps” in the control output when you switch from manual to automatic mode. Suppose you are messing with the system in manual mode, and then you switch to automatic mode. But because you were messing with the control output, the process variable could now be nowhere near the set point. That creates a large difference which can create a large sudden change in the output which could be hard on your system or possibly even dangerous. If you enable bumpless mode, and you are using the HMI for the set point, the drive simply copies the current process variable into the set point which guarantees there won’t be a large difference. Once PID is up and running you can then re-adjust the set point back to where you want it. We’ll leave that off for this demo just to keep things simple, but most of the time, you will probably want that enabled. Check out the Bumpless video to learn more about that feature. Each drive does this a little differently, but the video will give you a better understanding of the kinds of things to expect. The process variable is stored in engineering units in Parameter 40. Again, it’s grayed out to remind us it’s read only. We have a forward-acting system so we’ll leave that at the default. Forward or direct-acting means the pressure goes up when the motor speed goes up. A reverse-acting system would be like a cooling system where the temperature goes down when the motor speed goes up. We’re using Analog Input 1 for our process variable. This also enables PID. To disable PID set this to a zero. This guy creates a dead zone for small analog signals. We don’t want that messing with our PID calculations so leave it inactive. We don’t need to change the gain, we’re using the default 0 to 10V analog input, and don’t need an offset so we’ll leave all of those at the default blue values. I like to add a little filtering on my analog inputs to help reduce noise, but you want to keep this as small as possible because it will slow down the PID response. Learn more about Noise reduction in this video. Finally, we need to configure the display. We want to end up with the set point in psi on the first line of the display, because that’s the line that the keypads up-down arrow keys control. The process variable on the 2nd line also in psi, and the motor's current on the bar graph. The motor's RPM is always in the upper right so we get that for free. I marked all the display locations in red on our spreadsheet. Parameter 205 is what we want to show on the first line so we put the set point in engineering units there. If we wanted the percent value, then we would put this guy in here. We want a 15 psi scale with 1 decimal point so that’s a 150. We want the process variable in psi on the 2nd line of the display, so we put that here. And it uses the same scaling. Output current is the default for the bar graph and this drive can output 4.3 amps so we’ll leave those at the default too. Look! All the yellow cells are gone which means we are done configuring parameters. I went ahead and entered all of those into the drive to save us some time. Here’s our test station. I’m going to zoom in on the display and switches so you can see what I’m doing. Let’s start with PID in Manual mode – Remember, that’s where we bypass PID and we manually force the control output to the motor to whatever value we want it to be. I’ll switch to Run … and because the set point is currently zero the drive spins the motor up to the min output frequency we specified in Parameter 133, which comes out at this many RPMs. That min frequency we found in the previous video should give us close to zero psi and it does. If we manually increase the motor speed, nothing happens until we get to the minimum speed we put in Parameter 133, and then the RPMs and system pressure start going up. Perfect. I’ll adjust the motor speed to get the system pressure to 6 psi. And sure enough, this is the same RPM we found we needed in the previous video to maintain 6 psi with one valve open. I’ll open another valve. The system pressure drops. I’ll increase the RPMs to get back to 6 psi. Open another valve. System pressure drops, Increase the motor speed to get back to 6 psi. Open a third valve, same thing. This is exactly what we did in the previous video, isn’t it? We manually adjusted the motor speed to compensate for valves opening and closing. That’s what manual mode does – it allows us to manually control the system after PID is all set up. Let’s go back to 1 valve but I’m not going to adjust the speed to get back to 6 psi. We see the pressure went way up. Instead, let’s simply switch to Automatic mode and let PID do it for us. And yep, PID automatically adjusts the motor speed to get the system back to 6 psi. Open a second valve – and PID automatically adjusts the motor speed to compensate almost as fast as I can switch the valve! 3 valves, same thing. PID automatically compensates. And 4 valves, same thing. What if I want to run the system at 5 psi. No problem, just change the set point, and as quick as I can change it, PID automatically adjusts the motor speed to compensate, regardless of how many valves I have open. How about 7 psi. Same thing. PID automatically adjusts the motor speed so that no matter how many valves I open or close, the system automatically maintains 7 psi. So that’s it. You should now have a pretty good idea of how to get PID up and running on a WEG CFW500 Variable Frequency Drive. You’ll find a link to this configuration tool, wiring diagrams, etc., in the YouTube description below the video. Meanwhile, click here to learn more about the WEG CFW500 family of variable frequency drives. Click here to learn about AutomationDirect’s free award-winning support options and click here to subscribe to our YouTube channel so you will be notified when we publish videos like this one.
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
Site Map    Send Us your Feedback    Unsubscribe    Email Preferences    Legal & Business Policies    Cookie Preferences    YouTube Terms of Service    AutomationDirect Product API
Clear login credentials
Back to Top


 Updating...
Info