(VID-BRX-0008)
Introducing the newest family of Do-more PLCs
The BRX. This video reviews the contents in the BRX starter PLC kit. So, if you need a budget PLC or a large installation the BRX PLC has you covered.
This starter kit is perfect for someone looking for a PLC Training kit.
Our FREE Practical Guide to Programmable Logic Controllers eBook: https://go.pardot.com/l/548202/2018-08-06/7n3v42
Let’s see the goodies that comes with The BRX starter kit. When you open the box. You will first find the 30 day free training coupon for interconnecting automation, don’t lose that is a great freebie. It is a huge help in getting you started in the Do more designer software environment. The Software and manuals are also included on both CD and a USB storage card. This usb card is a very cool feature. Just flip this over and it will plug directly into your usb port. Also here is a QR code that will link you directly to our video library on the Do-more and Brx platform. Even before you get to the PLC, in this box, there is 4 ways that will make your experience successful. Now you will find the Plc, already mounted on din rail with a Power supply, that is pre-wired to run right out of the box. Just plug it up and get connected, to your PC. If you want to get connected over USB There is this USB POM module and cable that can install into the PLC and allow it to program over USB. There are more accessories in the box, as you notice the BRX PLC comes installed with the Spring clamp terminals. If you prefer to use the Zip link field wiring module or screw terminals, those can be found in the bottom of the box. Also in the bottom of the box you can find a SD card ( for data logging), a screwdriver and the all of the product inserts for the components of this kit. When you install the Do more Designer software, the start page is populated with these videos. They are great at getting you familiar with the programming environment. The software is free and available to download from our website, at any time. There are many ways in this one single box of helping you spend less and Do more. If you need any help with using an Automation Direct device please contact Automation Direct’s free, award winning Technical support team during regular business hours – they will be happy to help. And don’t forget the forums. There are lots of folks there that love to share their years of experience. Just don’t post questions directed at Automation Direct’s Technical support staff there, they do not monitor the forums on a regular basis.
Voted #1 mid-sized employer in Atlanta
Check out our
job openings