(VID-PN-0012)
BVS series modular solenoid air valves are 3-port (3-way) poppet valves in 2-position, normally open or normally closed configurations. BVM series modular solenoid valve manifolds simplify the mounting and wiring of BVS series valves.
Our FREE Practical Guide to Pneumatics eBook: https://go.pardot.com/l/548202/2018-08-06/7mysll
Welcome to Kickstart where you get to see new products here at AutomationDirect. Today I am going to show you our new line of NITRA pneumatic modular valves. Now AutomationDirect started carrying pneumatic products over a year ago. And our customers have been asking for more and more pneumatics so that we can become your ONE STOP SHOP. So, what we have here are called “Modular Control Valves”. These are a 3 way, 3 port poppet valve. 2 position, single solenoid, with normally open or normally closed spring return. And these come in a 12 volt DC, a 24 volt DC, or 120 volt AC coils. Now, if you’re mounting these they have panel-mount holes and we’ll zoom in on that in a second. Or, if you’re wanting to use a manifold, I’ll let you zoom in right now. And you can see here, you can panel-mount the manifold or on the back it has clips for DIN-rail. And that’s what we’ve done with this one. While you’re zoomed in, here are the holes for panel mounting a single, LED for indication and also the manual operator button. Now these can be wired a couple of different ways. If you are using them individually you can use the flying leads like these and they come with the leads. Or, if you are using a manifold, you can use the nice DB9 Ziplink Cable like what we have here. It makes wiring multiple valves SO much easier. These manifolds come in a couple different sizes so take a look at them on our web site. These are all made in the USA, there is no need for fittings because they all come with 4 millimeter push to connect tube fittings, and they are very small and lightweight and need minimum tools to require installation. I’ll show you real quickly, I have a 4 port manifold here, just added a second one, and since we aren’t populating the whole manifold you have to put in blanking plates like what I just did there. So this one is ready to go other than wiring it up. These all come with a 2 yr warranty. There is a total of 15 new part numbers with these new valves, manifolds and cables in this lineup. And you can find the agency approvals and specs for these modular pneumatic valves on our website at : www.automationdirect.com And don’t forget: we sell all kinds of other pneumatic parts such as tubing, fittings, valves, cylinders, hoses and more! Check back with us often on AutomationDirect’s websites or on Youtube.com/AutomationDirect for more Kickstart videos. And if you are watching with us today on YouTube, please let us know what you think about these products or how you plan to use these products in your next application by dropping us a comment down below. Thanks for watching and we hope to see you again soon.
Voted #1 mid-sized employer in Atlanta
Check out our
job openings