Cookies are not enabled on your browser.ADC will be closed Friday, July 3rd, to celebrate Independence Day. Orders placed after cut-off times on Thursday will be processed and shipped on Monday, July 6th.
To learn more: https://www.automationdirect.com/digital-panel-meter?utm_source=XXFsjuOT4cg&utm_medium=VideoTeamDescription
(VID-PS-0013)
In this how to video, we will cover the basics of configuring input types for the Prosense digital panel meters. We use a DPM3 meter, and will also setup a DPM2 and a DPM1 model in this same video.
Online Support Page: https://community.automationdirect.com/s/?utm_source=XXFsjuOT4cg&utm_medium=VideoTeamDescription
**Please check our website for our most up-to-date product pricing and availability.
In this HOW TO video, we will cover the basics of configuring input types for the Prosense digital panel meters. I am currently using a DPM3 meter, and we will also setup a DPM2 and a DPM1 model in this same video. On the DPM3 meter, first, I press the Enter button and it displays Pro for Program mode, I press the right arrow button and the first selection is CnInp for control input, I press Enter, and can scroll through the input types. We want process control, so we press Enter when we see ProC. We have two options; 20ma or 10v, I select 20ma and press Enter and we return to Program mode and now I press Enter one more time and the panel stores my selections into memory. We are now setup with a 4 to 20ma input in a DPM3 meter. Now let's configure the input for the DPM2 panel with a 4 to 20ma input signal. I press the Enter button and it displays Program mode, Press Enter again and it displays InP for inputs, press Enter again and you will now see ProC for process control and we scan scroll through the various input types like temperature, potentiometers and resistance. If we wanted to setup for temperature input, we select tEnP for temperature, press Enter and we see options for thermocouple or RTD. We select PT1 for RTD and Enter and now the panel displays in Celsius with a tenths decimal place. We can use the right arrow button to scroll through selecting Fahrenheit or Celsius and if we chose to use a decimal place. We press Enter and it allows us to select an offset. We choose zero, press Enter and its stores our setup. Now we get the Error message oUE for over since we currently have a 4 to 20ma input signal and NOT an RTD input. So, let's setup for the correct input: 4 to 20 mA. I press the Enter button and it displays Program mode, Press Enter again and it displays InP for inputs, press Enter again and you will now see ProC for process control. And we press Enter and now we have amperage or voltage. We select A for Amperage and press Enter, the display returns to Store. Now we are setup for a 4 to 20 ma input signal on our DPM2 model. Now let's configure a DPM1 model for amperage. The DPM1 models must be selected based on their input type whereas the DPM2 and DPM3 typically offer multiple input types. This unit accepts amperage and voltage only. As you notice, the smaller, DPM1 units do not have buttons on the face but instead have them on the bottom of the panel. There are still 3 buttons and they are still in the same configuration as the other two models. First, we press Enter and it displays Pro for Program. I press Enter again and it quickly displays Inp for INPUT and switches to A for amperage. I use the middle button to scroll through the input types until I get to the desired input type. We want amps, so I scroll until I see A. I press Enter, and we read disp then it quickly switches to scal for scale. I don't wish to scale in this setup, so I will leave it at the default by pressing Enter. Inp1 for input 1 and 04.00 displays. We are using a 4 to 20ma input, so we leave this one alone. Enter and DsP1 displays with 04.00. Enter and now we can adjust our decimal point. Enter and InP2 displays 20.00. Enter and Dsp2 displays 20.00. Enter and now the input type is stored into the unit. Now let's configure a DPM1 T model for temperature. This one is connected to an RTD. First press Enter and we see Pro for program, press Enter and now we can scroll through the different temperature input types. I select P100 for this one because I have an RTD connected. Press Enter and we can select if we want to use a decimal point. Press Enter and we can select Celsius or Fahrenheit, then Enter and we can choose an offset. I leave this one at zero, press Enter and the value is now stored. This is how you setup input types in the DPM1, DPM2 and DPM3 Prosense Digital panel meters. I hope you found this video useful and follow us to our other How to videos on the ProSense Digital Panel Meters. Thanks and have a great day.
Voted #1 mid-sized employer in Atlanta
Check out our
job openings