Cookies are not enabled on your browser.
To learn more: https://www.AutomationDirect.com/pneumatics?utm_source=_bR5iWfSIlw&utm_medium=VideoTeamDescription
(VID-RB-0007)
This automated trophy was created for the 2019 FIRST Robotics Destination Deep Space FRC game. The trophy features NITRA pneumatics that uses no electronics to create a memorable trophy for the 2019 Georgia FIRST Robotics off season GRITS event.
Design files for this trophy are located here:
https://cdn.automationdirect.com/static/video-resources/robotics/grits_trophies/trophy-design-files/GRITS-2019-Trophy-Design-(Destination-Deep-Space).zip
Visit www.GAFIRST.org for more information about Georgia FIRST.
Visit www.firstinspires.org to learn more about FIRST robotics.
Online Support Page: https://community.automationdirect.com/s/contactsupport?utm_source=_bR5iWfSIlw&utm_medium=VideoTeamDescription
**Please check our website for our most up-to-date product pricing and availability.
The 2019 interactive GRITS trophy created by AutomationDirect allows you to simulate the end of the game by launching either the red rocket … or the blue rocket. And … if you hold one of the rockets in the launch position, and then switch to auto, the trophy automatically launches the rockets. This trophy design is unique because there are no electronics controlling any of this. These buttons switch airflow, not electric current. This selector switch also switches airflow. If I turn the trophy over, you can see when the piston comes down, it hits this pneumatic switch which switches the airflow in automatic mode to send the rocket back up. We’ve included a plumbing diagram that shows how all of this is connected. See if you can follow the airflow and figure out how it works! Of course, it depends heavily on proper air flow through the system, so there are also instructions telling you how to calibrate the airflow which will also give you some hints on how this works. For example, for this to work the rockets have to rise faster than they fall. See if you can figure out why that is! Imagine being able to control some of your robot functionality with pneumatics only circuits! Learn how this trophy works and you will be well on your way towards doing exactly that with these cool pneumatic parts from AutomationDirect!
Voted #1 mid-sized employer in Atlanta
Check out our
job openings