AutomationDirect
Login | Register
Accounts & Orders
Cart
13
$2,992.50

Recent Orders

View and Manage | Request Cancellation
Loading Order History
Loading...

Your Account

Account Home

Checkout   $2,992.50
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
Videos Home > Magnetic Flow Meters Overview ...

Magnetic Flow Meters Overview from AutomationDirect


Related Products

FMM50-1002
FMM50-1002 Thumbnail
FMM75-1002
FMM75-1002 Thumbnail
FMM100-1002
FMM100-1002 Thumbnail
FMM150-1002
FMM150-1002 Thumbnail
FMM200-1002
FMM200-1002 Thumbnail
FMM50-1001
FMM50-1001 Thumbnail
FMM75-1001
FMM75-1001 Thumbnail
FMM100-1001
FMM100-1001 Thumbnail
FMM150-1001
FMM150-1001 Thumbnail
FMM200-1001
FMM200-1001 Thumbnail
FMM-GND1
FMM-GND1 Thumbnail


To learn more: https://www.automationdirect.com/flow-sensor?utm_source=lM9ScEQJLYQ&utm_medium=VideoTeamDescription

(VID-FL-0002)

Learn how Magnetic Flow Meters work, what you can do with them and which ones AutomationDirect offers. Check out the other flow meter videos to see how to get up and running quickly!

Online Support Page: https://community.automationdirect.com/s/?utm_source=lM9ScEQJLYQ&utm_medium=VideoTeamDescription

**Please check our website for our most up-to-date product pricing and availability.


Hide Transcript
View Transcript

Magnetic Inductive Flow sensors from AutomationDirect are an excellent way to measure liquid flow rates in half inch to 2 inch NPT pipes up to 160 gallons per minute. And because there aren’t any moving parts, they give you a robust, accurate and easy way to measure the flow rate of conductive fluids including viscus fluids and slurries. The liquid flows through a magnetic field in the sensor inducing a voltage with is proportional to the flow rate of the liquid. The faster the liquid moves, the bigger the voltage. Of course, for that to work, the liquid you are measuring has to have some conductivity. Here’s a chart showing the relative amounts of conductivity of different kinds of water based fluids. It doesn’t matter how much conductivity the fluid has – as long as it has some conductivity greater than 20 micro-siemens the sensor will figure it out and provide the proper flow rate. The beauty of this is there is no calibration or inputs you need to provide, the sensor automatically takes care of all of that. There are two versions in this family of sensors. The 1001 series has configurable digital outputs on channel 1 for flow sensing and switched or analog options on output 2 for flow or temperature or it can be used as a reset input. The 1002 series only has the two 4-20mA analog outputs for measuring temperature on channel 1 and flow on channel 2. So it’s easier to setup because there is nothing to configure on the outputs. Output 1 on the 1001 Series can be set up as a switch to indicate some limit has been reached to shut off a valve or signal an alarm, or as a pulse that triggers every time a specified number of gallons passes by for counting applications, and the two larger models can also be setup with a frequency output. Output 2 on the 1001 series can be setup as a switched output or an analog output for Flow or Temperature. Output 2 can also be used as an input to reset output 1. The digital outputs can be setup for NPN or PNP, and N.O. N.C. and are short circuit protected – non-latching. The frequency output is handy if you need to replace another type of sensor like a paddle wheel that outputs a frequency signal. Magnetic Inductive flow meters with a frequency output allow you to drop this sensor right in place of the other type of sensor and not have to change any of your existing electronics! And since the Magnetic Inductive Flow sensor doesn’t have any moving parts and doesn’t have things like paddle wheels impede the flow of your fluid, you will have a much more reliable and hassle free system. The built in LED display and push buttons make setup quick and easy. There’s no need for special configuration software or download cables. And it can be set for Gallons per minute, gallons per hour, total gallons and you can even view the temperature of the fluid. Here’s a chart that summarizes the Process connection size, Flow range, outputs available and if the sensor has empty pipe detection. They all operate over minus four to 176 degrees F and have the same display options. They are all class three, so they don’t require a ground – which is handy if you are using them in a PVC pipe installation. So if you need to reliably measure the flow rate or flow volume of a conductive fluid, check out these Magnetic Inductive flow rate sensors from AutomationDirect. And be sure to watch this brief quick start video to get up and running quickly. If you have any questions, please contact AutomationDirect’s free award winning tech support team during regular business hours. They will be happy to help you. And don’t forget the forums. There are lots of folks there that love to share their years of experience. Just don’t post any questions for AutomationDirect’s support team there – they don’t monitor the forums in a regular basis.
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
Site Map    Send Us your Feedback    Unsubscribe    Email Preferences    Legal & Business Policies    Cookie Preferences    YouTube Terms of Service    AutomationDirect Product API
Clear login credentials
Back to Top


 Updating...
Info