Cookies are not enabled on your browser.
To learn more: https://www.AutomationDirect.com/https://www.automationdirect.com/sure-servo2/?utm_source=qn6kqy_fnb4&utm_medium=VideoTeamDescription
(VID-SV-0097)
The SureServo2 lineup has a ton of functionality in its position and velocity modes, but what happens when you need to set a variable position or velocity but target a specific torque? Maybe you need to run a precision unwinder or draw wire to a specific gauge thickness. These are high-precision torque applications that are beyond the ability of a normal VFD and motor. The SureServo2, however, shines. Watch our 2-part video series and see what it's all about.
SureServo2 Pro Software version 0.0.4.13 used
Part 1 of this series: https://www.automationdirect.com/VID-SV-0087?utm_source=qn6kqy_fnb4&utm_medium=VideoTeamDescription
Online Support Page: https://community.automationdirect.com/s/?utm_source=qn6kqy_fnb4&utm_medium=VideoTeamDescription
**Please check our website for our most up-to-date product pricing and availability.
The SureServo 2 platform offers many options for application flexibility. Many of the modes are position-based; however, the drive offers an option to run the motor at a specified torque up to a preset speed. A high-quality servo will greatly outperform a traditional VFD and motor for precision torque output. Let’s take a look at “torque mode” in the SureServo2 today. To help with seeing the timing on all this, let’s do a little sports-style picture-in-picture and show the motor and actuator, the drive face, and the software all at the same time. Let’s output a 65% Torque level to start the motion base moving upwards. If we add a 1-kilogram weight, we see it reduce speed as it comes to equilibrium at 65% of torque. Now let’s add another 500 grams of weight, and we see that since it wants to stay at the 65% torque value, it decreases speed to compensate, and in this case has come to a standstill. The motor is still engaged and outputting torque. If we change the torque level to 100% of motor rated torque, it immediately resumes moving again, even with the added weight, as we have allowed the system to output more torque. If you liked this video, give it a like and check out our long-form two-part SureServo2 Torque mode video set here… To subscribe to our YouTube channel, click here… To visit our webstore for SureServo2 products, click here… If you want to see more SureServo2 videos, click here…
Voted #1 mid-sized employer in Atlanta
Check out our
job openings