(VID-DD-0070)
This video gives basic information on Using the FILESYSCMD "Perform File System Command" instruction in the Do-more Designer software. It presents information that is commonly missed by users. This WILL NOT be a complete tutorial for the instruction but rather a supplement to the help file and customer experience.
Our FREE Practical Guide to Programmable Logic Controllers eBook: https://go.pardot.com/l/548202/2018-08-06/7n3v42
This instruction is used to apply three different commands to the File System. The first is format. This will remove all files or folders on the RAM file system. The format option is not valid for the SD cad System. Dismount prepares the SD card for extraction. It closes all the files, ends outstanding file operation and the memory light on the BRX CPU will turn red. The mount prepares the SD card File system for use. With the card installed, and the mount function triggered the memory light on the BRX CPU will turn green. This instruction can be used in a Task or Program but cannot be used in Subroutines or Interrupt service routines. Now only BRX PLCs have the SD Card File System, but all Do-mores have a useable RAM File System if they have above version 2.0 firmware.
Voted #1 mid-sized employer in Atlanta
Check out our
job openings