AutomationDirect
Login | Register
Accounts & Orders
Cart
2
$95.00

Recent Orders

View and Manage | Request Cancellation
Loading Order History
Loading...

Your Account

Account Home

Checkout   $95.00
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
Videos Home > IronHorse Helical Gearbox DIY ...

IronHorse Helical Gearbox DIY Install & Maintenance from AutomationDirect


Related Products

HGR-37-010-B
HGR-37-010-B Thumbnail
HGR-37-015-A
HGR-37-015-A Thumbnail
HGR-37-015-B
HGR-37-015-B Thumbnail
HGR-37-020-A
HGR-37-020-A Thumbnail
HGR-37-020-B
HGR-37-020-B Thumbnail
HGR-37-030-A
HGR-37-030-A Thumbnail
HGR-37-030-B
HGR-37-030-B Thumbnail
HGR-37-040-A
HGR-37-040-A Thumbnail
HGR-37-060-A
HGR-37-060-A Thumbnail
HGR-47-005-B
HGR-47-005-B Thumbnail
HGR-47-005-C
HGR-47-005-C Thumbnail
HGR-47-010-C
HGR-47-010-C Thumbnail
HGR-47-015-C
HGR-47-015-C Thumbnail
HGR-47-020-B
HGR-47-020-B Thumbnail
HGR-47-020-C
HGR-47-020-C Thumbnail
HGR-47-030-B
HGR-47-030-B Thumbnail
HGR-47-030-C
HGR-47-030-C Thumbnail
HGR-47-040-A
HGR-47-040-A Thumbnail
HGR-47-060-A
HGR-47-060-A Thumbnail
HGR-67-005-B
HGR-67-005-B Thumbnail
HGR-67-005-C
HGR-67-005-C Thumbnail
HGR-67-010-C
HGR-67-010-C Thumbnail
HGR-67-015-B
HGR-67-015-B Thumbnail
HGR-67-015-C
HGR-67-015-C Thumbnail
HGR-67-020-C
HGR-67-020-C Thumbnail
HGR-67-030-B
HGR-67-030-B Thumbnail
HGR-67-040-B
HGR-67-040-B Thumbnail
HGR-67-060-A
HGR-67-060-A Thumbnail
HGR-77-005-C
HGR-77-005-C Thumbnail
HGR-77-005-D
HGR-77-005-D Thumbnail
HGR-77-010-D
HGR-77-010-D Thumbnail
HGR-77-020-C
HGR-77-020-C Thumbnail
HGR-77-030-C
HGR-77-030-C Thumbnail
HGR-77-040-C
HGR-77-040-C Thumbnail
HGR-77-060-B
HGR-77-060-B Thumbnail
HGR-87-005-D
HGR-87-005-D Thumbnail
HGR-87-005-E
HGR-87-005-E Thumbnail
HGR-87-010-D
HGR-87-010-D Thumbnail
HGR-87-015-D
HGR-87-015-D Thumbnail
HGR-87-020-C
HGR-87-020-C Thumbnail
HGR-87-020-D
HGR-87-020-D Thumbnail
HGR-87-030-C
HGR-87-030-C Thumbnail
HGR-87-040-C
HGR-87-040-C Thumbnail
HGR-87-060-B
HGR-87-060-B Thumbnail
HGR-87-060-C
HGR-87-060-C Thumbnail
HGR-37-005-A
HGR-37-005-A Thumbnail
HGR-37-005-B
HGR-37-005-B Thumbnail
HGR-37-010-A
HGR-37-010-A Thumbnail


To learn more: https://www.automationdirect.com/power-transmission?utm_source=yEJVcSSNJJw&utm_medium=VideoTeamDescription

(VID-PT-0002)

In this how to video, we cover the basics of installation and maintenance on an IronHorse helical gearbox. Currently AutomationDirect offers Cast Iron and Aluminum Worm Gearboxes as well as Cast Iron Helical Gearboxes.

Online Support Page: https://community.automationdirect.com/s/?utm_source=yEJVcSSNJJw&utm_medium=VideoTeamDescription

**Please check our website for our most up-to-date product pricing and availability.


Hide Transcript
View Transcript

In this How To video, we will cover the DIY basic install and maintenance of our IronHorse Cast Iron Helical Gearboxes. Before we get started lets discuss safety. Prior to working on any mechanical or electrical device, please make sure you are wearing proper PPE. To minimize the risk of potential safety problems, you should follow all applicable local and national codes that regulate the installation, maintenance and operation of your equipment. Studies state that Helical Gearboxes are the most commonly used gear in transmissions. Helical gearboxes offer less vibration, wear, noise and tend to have a longer life. If you are trying to select the proper gearbox for your application, please refer to our IronHorse Gearbox Selection video, the Selection Guide or call our Free, Award winning technical support. These can all be found on our website at AutomationDirect.com. In the following discussions, I refer to the user manual: IH-HG-USER-M-WO. You can find this manual on our website at AutomationDirect.com. Prior to Installation, we need to decide: how will the gearbox be mounted in order to determine the placement of the vent plug and what hardware and accessories will be required for proper mounting. First, we inspect the gearbox for any damage that may have occurred during shipment. Clean the gearbox if needed now and during maintenance. Do not allow chemicals on the seals as they can cause seals to deteriorate and leak. Our Cast Iron Helical models include a vent plug that may be plastic like this one, or brass like this one. The vent plug is included with our Helical Gearboxes and is attached during shipping. Depending on the gearbox mounting orientation, we may need to move where the vent plug is installed. All IronHorse Helical Gearboxes have six filler/oil gauge/drain plug locations. These plugs are located in different locations depending on the actual box size selected. The vent plug should be installed in the filler position as specified in the user manual. The plug in the oil gauge location should be removed while filling with oil. Oil has reached the proper level in the gearbox when it starts to drip out of the gauge port. After filling, plug the gauge port and install the vent plug in the filler port. If your vent plug is plastic, remove the red pin from the plug. This red device closes the breathing hole so oil does not leak out during shipping. The brass plug only needs to be installed and it is ready to go. Mounting instructions can be found in the user manual on this chart. The Helical Gearbox can be placed in any of five install positions. M2 mounting position where the gearbox output shaft is vertical pointing down is not permitted. This same chart informs the user where the filler, oil gauge and drain plugs should be located depending on mounting orientation. All IronHorse Helical Gearboxes are tested and filled with lubricant prior to shipping. Oil may need to be added or partially drained depending upon your mounting orientation. Make sure you don't add too much oil because it will cause overheating and can cause seals to leak while too little oil will result in gear failure. To insure the proper amount of oil, mount the gearbox, determine the vent plug, gauge and drain plug locations and fill or drain the oil to the proper amount recommended in the user manual. It is very important to use the proper lubricant when adding or changing the oil. Recommended oil types and brands are specified in the user manual. These IronHorse Helical Gearboxes do not require a run in procedure; however the oil should be changed after the first 300 hours of operation and then every 2500 hours or every 6 months, whichever comes first. It is recommended to use an anti-seize compound on hollow output shafts. Once the gearbox is installed and tested the gearbox temperatures should be monitored during initial operation. If the temperature exceeds 80 degrees Celsius (that's 176 degrees Fahrenheit), check for overloads, high ambient temperatures and proper venting. You can find the specs for these IronHorse Helical Gearboxes on our website at: www.automationdirect.com Don't forget: we sell Worm Gearboxes, Motors, Motor controls and more. If you need any help with selecting a gearbox or have questions, please contact Automation Directs free, award winning Technical support team during regular business hours, they will be happy to help. And don't forget the forums. There are lots of folks there that love to share their years of experience. Just don't post questions directed at Automation Directs Technical support staff there, they do not monitor the forums on a regular basis. Thanks for watching and we hope to see you again soon.
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
Site Map    Send Us your Feedback    Unsubscribe    Email Preferences    Legal & Business Policies    Cookie Preferences    YouTube Terms of Service    AutomationDirect Product API
Clear login credentials
Back to Top


 Updating...
Info