Filter Results Clear All
You've selected:
> Communications > Secure Remote Access - VPN > VPN Routers
  •   Shop  
  •   Overview  
  •    In Depth   
VPN Routers
VPN Routers

StrideLinx VPN routers provide an outgoing, secure connection from remote machines or systems to the StrideLinx cloud platform, available in wired, wireless, and cellular models with a built-in firewall to isolate company and control networks.

Stride Interactive Product Tour Request
Company Name:
Last Name:
First Name:
Business Email:
Country:
Job Title:
Category Selections
VPN Routers
VPN Routers
Newest Additions!
Antennas
Antennas
Newest Additions!
Cloud Services
Cloud Services
Newest Additions!
Shop Now

Secure Remote Access - StrideLinx VPN Routers

Category Selection

  • Wired/WiFi Industrial VPN Router
  • Wired/Cellular Industrial VPN Router
  • Wired Industrial VPN Router

The StrideLinx router acts as an industrial IoT gateway by providing remote access and remote data capabilities. Simply place the StrideLinx router near your machine or process and connect devices like PLCs or HMIs directly to it. Once the router automatically connects to the StrideLinx server network, you can then link to the remote devices through a secure VPN connection as if you were directly connected on-site.

The StrideLinx routers are available with Wired, WiFi, or 4G LTE connectivity. They are also equipped with a built-in configurable firewall that provides complete isolation between the control network (LAN) and the company network (WAN). Only authorized and encrypted data verified with a valid certificate will be allowed to pass. This network separation ensures that users with remote access can only access the LAN side of the network and not the rest of the network.

Industrial VPN router connections:

  • 4G model uses a standard SIM (2FF) card for 4G LTE Verizon, AT&T or T-Mobile cellular connections (AT&T SIM card included with router). Great for sites where Internet connections may not be readily available
  • The antenna connectors (4G/WiFi models) are standard SMA screw connectors with 5 antenna options available
  • USB 2.0 port for easy router configuration using the included USB drive
  • Four RJ45 Gigabit Ethernet ports for extremely fast data transfer to/from PLCs, HMIs, drives, or any Ethernet-capable control device
  • One RJ45 Gigabit Ethernet port for connectivity to a company-wide network
  • The SE-SL3011- 4GG supports a wide choice of worldwide LTE frequency bands

Simple Setup

With the StrideLinx router's easy 3-step configuration, you can cloud-enable your machine in as little as 2 minutes.

  1. Log in to your company account and using the web-based dashboard within the platform, configure the router's parameters.
  2. Download the parameter file to the provided USB drive.
  3. Install the USB in the router and it will automatically authenticate and connect to the proper account on the platform. This USB can then be used on any other router that needs to be configured for the same company account.

Already have a cloud solution in place? With StrideLinx, that's no problem. StrideLinx supports data sharing directly from the StrideLinx router to several popular 3rd party MQTT brokers. Use low-cost StrideLinx routers to transmit your factory floor data to an established 3rd party platform where it can be processed, analyzed, visualized, and used in any way needed. Supported MQTT brokers include:

  • Azure IoT Hub
  • Azure Event Grid
  • Amazon Web Services (AWS) IoT Core
  • Eclipse Mosquitto broker
  • Self-hosted solution

For part listings and specifications, go to Shop Now

StrideLinx Industrial VPN Routers
(shown with antenna)

WiFi/Wired Industrial VPN Router

For applications where wireless connections are preferred, StrideLinx offers a WiFi capable router and (2) 2.4GHz WiFi antennas (one antenna is required). WiFi capable routers provide the ability to wirelessly connect to company networks and/ or wirelessly connect control devices to the router.

  • WiFi/Wired VPN router
  • DIN rail mount, metal case
  • Gigabit Ethernet (1000Mbps) port speed
  • 5 Ports (RJ45 for wired applications)
  • 2.4GHz antenna sold separately
  • Supports access point or client mode

Priced at
$652.00
(SE-SL3011-WF)

StrideLinx Industrial VPN Routers
(shown with antennas)

Cellular/Wired Industrial VPN Routers

For applications where Internet connections are not readily available, StrideLinx offers 4G cellular capable routers and LTE antennas. A SIM card and/or data plan will need to be purchased from the local retailer (AT&T SIM card is included with router).

  • Support for global 4G LTE frequencies and bands
  • DIN rail mount, metal case
  • Gigabit Ethernet (1000Mbps) port speed
  • 5 Ports (RJ45 for wired applications)
Verizon ready
AT&T

Priced at
$763.00
(SE-SL3011-4GG)

STRIDE StrideLinx Industrial VPN Routers

Wired Industrial VPN Routers

The StrideLinx wired-only router provides (5) Gigabit Ethernet ports for control devices and Internet connections. No additional components are required.

  • Wired basic router (SE-SL3001) offers a cost-conscious remote access option without data logging support
  • Wired Gigabit Ethernet (1000Mbps) VPN routers
  • DIN rail mount, metal case
  • Gigabit Ethernet (1000Mbps) port speed
  • 5 Ports (RJ45)
  • Easy, secure VPN networking

Starting at
$400.00
(SE-SL3001)


Shop Now