> Programmable Controllers > Do-more H2 & T1H PLCs (Micro Modular & Stackable)
  •   Shop  
  •   Overview  
  •   In Depth  
Do-more Home Download Free Software
 
Features
Top 11 Ways You Can Do More with this PLC Serial Communications Ethernet Communications High Speed Modules Hign Speed Inputs Motion Control Remote I/O Free Online Training
Free Software
Simulator Auto-Discover I/O Communications Powerful Math Monitoring & Troubleshooting Memory Management Program Management Project Management Security Download the FREE software
Hardware
H2 CPUs T1H CPUs Bases AC I/O Modules DC I/O Modules AC & DC I/O Modules Analog I/O Modules Specialty Modules Go to ZIPLink Selector Tool
Videos


Do-more H2 (Micro Modular PLC): Do-more Designer Videos

Detailed Product
Overview



To learn more: https://www.automationdirect.com/do-more?utm_source=lC8HHVQgYwk&utm_medium=VideoTeamDescription - (VID-DD-0014)

This video gives basic information on Using the FREQCNT "Frequency Counter" instruction in the Do-more Designer software. It presents information that is commonly missed by users.
** Software Version used in this video: Do-more Designer 2.0

Online Support Page: https://community.automationdirect.com/s/?utm_source=lC8HHVQgYwk&utm_medium=VideoTeamDescription

**Please check our website for our most up-to-date product pricing and availability.


Hide Transcript
View Transcript
This is a multi-scan instruction, because

it takes multiple scans to complete, it cannot be used in either Subroutines or Interrupt

Service Routines. It can used in Programs and under special

circumstances it can also be used in Stages inside of a Program or in Tasks. See the help topic “Instruction Set Chart”

for more information. This instruction takes input pulse counts

and converts them to a rate based upon the sample time and the Frequency units you select

here. If you find your output to be erratic, use

the filter, to smooth the reading. If the filter is not enough to smooth the

reading, try increasing the sample time.


BRX Do-more PLCs Do-more Designer Software & Programming
  • Video
    BRX Do-more Designer Using the CALL Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the ENDC Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the ENTASK Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the EXIT Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the GOTO Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the HALT Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the LABEL Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the REBOOT Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the RESTART Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the RET Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the RETC Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the INTCONFIG Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the INTDECONFIG Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the INTRESUME Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the INTSUSPEND Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the JMP Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the JMPI Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the RUN Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the STOP Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the SUSPEND Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the WATCHDOG Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the YIELD Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the SG Stage Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the SGCONVRG Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the SGDIVRG Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the SGRST Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the SGRSTR Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the SGSET Instruction from AutomationDirect

Playlist Not Found Could not find playlist PLPdypWXY_ROovolXmvgjO63qk2RdsoIGx

Playlist Not Found Could not find playlist PLPdypWXY_ROoIDZ7MO4OLz8AMJ_lExObe

Playlist Not Found Could not find playlist PLPdypWXY_ROoiFQetOa9Kc_9NF3dLgQon