AutomationDirect
Search
Login | Register
Accounts & Orders
Cart
1
$53.00

Recent Orders

View and Manage | Request Cancellation
Loading Order History
Loading...Loading...

Your Account

Account Home

Checkout   $53.00


  • My Orders
  • Product Returns (RMAs)
  • Pay Proforma Invoices
  • Pay Freights
  • Pay Invoices / Invoice Reprint
  • Quotes / Favs / BOMs
  • Packing List Reprint
  • Purchase History Reports
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
> Programmable Controllers > Do-more H2 & T1H PLCs (Micro Modular & Stackable)
  •   Shop  
  •   Overview  
  •   In Depth  
Do-more Home Download Free Software
 
Features
Top 11 Ways You Can Do More with this PLC Serial Communications Ethernet Communications High Speed Modules Hign Speed Inputs Motion Control Remote I/O Free Online Training
Free Software
Simulator Auto-Discover I/O Communications Powerful Math Monitoring & Troubleshooting Memory Management Program Management Project Management Security Download the FREE software
Hardware
H2 CPUs T1H CPUs Bases AC I/O Modules DC I/O Modules AC & DC I/O Modules Analog I/O Modules Specialty Modules Go to ZIPLink Selector Tool
Videos


Do-more H2 (Micro Modular PLC) Videos

View Do-more Designer Videos


Detailed Product
Overview



To learn more: https://www.automationdirect.com/do-more?utm_source=1K69iKDZEKk&utm_medium=VideoTeamDescription - (VID-DM-0010)

This video provides a quick review of the new enhancements in the DoMore Designer 1.1 release.

Online Support Page: https://community.automationdirect.com/s/?utm_source=1K69iKDZEKk&utm_medium=VideoTeamDescription

**Please check our website for our most up-to-date product pricing and availability.


Hide Transcript
View Transcript
Version 1.1 of the DoMore designer is a major

update and at AutomationDirect there is no cost for DoMore Designer updates so be sure

to download and install it - you’ll be glad you did. If you right click and copy a code block and

then right click again and say paste code block it now works exactly as you would expect

– it takes the previous code block makes an exact copy, changes the name by adding

the word COPY up front and and drops it right in place. You can then change the name of that new code

block by right clicking and saying “configure code block” and change the name, or down

in the output window, you can see a note here that we made a smart copy of a code block,

and to rename that code block just double click on the message above. And you get the same dialog. Change then name and you are good to go. That’s a quick and easy way to replicate

tasks and programs which is great if you have a machine with lots of similar functions. Of course, for that to work you have to be

in EDIT mode. Also, if you copy a section of code that contains

local references like this this Stage example right here, and then paste it in another routine,

you get a dialog giving you some options on how you want things to be handled. You get to specify if how the documentation

should be handled and you can specify if you want all the references to change to the new

code block. I do in this case, so I say Paste it. And sure enough, I get my new stage program

and look – all the references refer to the new program, not the old one. Exactly what I wanted, perfect. There’s a new status bit called $EthMasterError

that tells you when something is amiss in the Ethernet I/O system. You just keep an eye on that and when it lights

up you can then run a routine that will analyze the system and pin point the issue. You can do that by working your way down this

$EthIOMaster structure which has detailed status on every component in the entire Ethernet

I/O system. Note that this new Ethner Master Error Flag

also lights up the yellow warning that you get down at the bottom of the screen sometimes. This new $EthMissedFrames gives you a count

of the number of Ethrnet Frames that were ignored during a data storm due to limits

on packet queue lengths. You’ll want to keep an eye on that as a

good indicator of Etherenet System Health. Stage programming now automatically increments

the stage number. So if you have a stage here and another one

here, and you add a stage – look, it automatically knows what the next stage is and populates

that for you. I use a lot of stage so I really like that

one. Both the Cross reference and Documentation

editor now allow you to pick a sort order. If you have a favorite sot order that you

want them to default to, just go into View >> Options, select the tab for the cross reference

or the documentation editor and pick the default sort order right here. All of the items in in all three panels of

the launch pad now have right click context sensitive menus. So you can right click and and you can see

exactly what you can do with each element in any of the paynes. Nice. The DoMore defaults to listening for other

DoMores on port 0x7070. You can now configure a second port if you

want to by going to Configre >> CPU >> and enable it right here and put the port number

righ there. Note that this is decimal, you’ll see the

hexidecimal version right here. Once you have the CPU configured, don’t

forget that you also need to configure the link. So when you connect to a PLC – I’m going

to edit this one since it is already existing – under the Port Tab >> select Ethernet,

UDP/IP. You can enter your Ethernet Address here. Under Advanced settings, you can configure

that alternate port number. Again, this is a decimal number. When you bring up the element browser you

get a list of all of the nicknames for all the elements in the entire system which you

could pair down by turning off the system nicknames if you want to. But in a large project your going to have

a lot of nicknames here. So it still may not be enough. So if you want to pair that down more, there

is a new filter right here that says filter on selected range. What that does, is now when you click on a

range of elements, it only showes you the nicknames for that range. Here are all the output coils for example,

and here’s the contacts. Very cool. Normally when you bring up a cross reference

it lists all the elements in your project with one exception – ranges of elements

like we have in the Reset Range of elements dialog right here. It starts at C10 and goes through C20. With version 1.1 though, you now see that

range. And if you hit this expand button, expand

button, you see all the elements in that range. That’s really great because now you can’t

accidentally re-use an element just because it was hidden in a range! It used to be that you could right click and

under this debug code bolck menue you could suspend or unsuspend a code block. With version 1.1 – when you right click

and say debug code block - you can actually run a program, trigger a task if that’s

what you right clicked on, or halt a program or task. That makes it really quick and easy to control

different programs and tasks that are buried someplace in your project. That’s really handy. Note this only works if you are connected

to a PLC. If I disconnect, and try the same thing, that

debug menu is gone – isn’t it? Youv’e always been able to zoom in or out

in your ladder logic, just by doing a control shift num plus or a control shift num minus. Wouldn’t it be great though, if you could

have all new views in a project start at that same zoom level? Now you can – if you go up to View >> Options

and look under the ladder tab, you can now set the default zoom level to anything you

want. When you get a program that has lots of tasks

and programs in it, it starts to get hard to figure out where each one is used and to

find it when you need it. Well look at this, now if you right click

on the task or program, and there is this new cross reference and it lists every place

that task is used. And if you click on it – it takes you directly

to the usage of that task or program. I use a lot of programs and tasks, so that

makes my life a whole lot easier! Keep in mind that is only going to work the

way you expect it to after you have accepted all of your changes. When you get errors and warnings in the output

window, what happens if you double click on one of the items? Well, look at this – now if you select any

item, you get a little message right here that tells you exactly what will happen when

you double click. In this case, if you double click, it will

go directly to the coorresponding address in that code block. All of the enhancements covered in this video

and the New Features video are detailed in a PDF which you can quickly get to by clicking

on this star right here. Be sure to check that document for more details

on what you have seen in this video. Many of the enhancements you’ve seen in

this video came from users like you. AutomationDirect and Host Engineering take

feedback seriously, so please keep those suggestions coming! How do you do that? Right here – under help, support – look

it will take you directly to Automation Direct support, the automationdirect forum or the

Host engineering forum. Drop them a note – they really appreciate

the feedback – both the good and the bad! Check out the other DoMore videos in this

series for more ways to get the most out of your DoMore system. And don’t forget – Automation Directs

tech support is FREE and you will talk to a real live person here in the US within minutes. Got a question? You can call, e-mail, or even do on-line chat

during regular business hours. Spend LESS. Do MORE. From Automation Direct


Playlist Not Found Could not find playlist PLPdypWXY_ROoEcDCcD10Qdb3S9tOmfEn5

Playlist Not Found Could not find playlist PLPdypWXY_ROoJx-HnK9gj2Z5a-i7th-UK

Playlist Not Found Could not find playlist PLPdypWXY_ROqvbaYVBWc3kH-pP01fI4-E

Playlist Not Found Could not find playlist PLPdypWXY_ROr5OPw3e0o8rLC0JQijmCNY

Playlist Not Found Could not find playlist PLPdypWXY_ROrtSkGYNq8Xc52QWTCWf2Ci

Playlist Not Found Could not find playlist PLPdypWXY_ROrRJ5YuFYxs3mSXr9250AN7

Playlist Not Found Could not find playlist PLPdypWXY_ROqJO86ikigKmjnSkbguBKBw

Playlist Not Found Could not find playlist PLPdypWXY_ROqWWy8OnWGt3YD4Dald6uf-

Playlist Not Found Could not find playlist PLPdypWXY_ROrmjIdXLaeovoTLZP65hdac

Playlist Not Found Could not find playlist PLPdypWXY_ROoqTZihvX8c8UUj5GzVCuKH

Playlist Not Found Could not find playlist PLPdypWXY_ROr0ZfCV-fAgau5yDemA19CV

BRX Do-more PLCs - Motion Control & High Speed Inputs
  • Video
    BRX Do-more CTRIO2 Motion Demo Hardware from AutomationDirect
  • Video
    BRX Do-more CTRIO2 Motion Config & JOG from AutomationDirect
  • Video
    BRX Do-more CTRIO2 Motion Dynamic Motion from AutomationDirect
  • Video
    BRX Do-more CTRIO2 Motion Using Limits from AutomationDirect
  • Video
    BRX Do-more CTRIO2 Motion Trapezoid Moves from AutomationDirect
  • Video
    BRX Do-more CTRIO2 Motion Using Encoders from AutomationDirect
BRX Do-more PLCs - Hardware
  • Video
    How To Sense Temperature with a Do-more PLC from AutomationDirect
  • Video
    How To Detect Objects with an AutomationDirect Do-more PLC
  • Video
    AC Motor On/Off with Do-more PLC Part 1 from AutomationDirect
  • Video
    AC Motor On/Off with Do-more PLC Part 2 from AutomationDirect
  • Video
    How to Sense Distance with an AutomationDirect Do-more PLC