AutomationDirect
Search
Login | Register
Accounts & Orders
Cart
1
$40.50

Recent Orders

View and Manage | Request Cancellation
Loading Order History
Loading...Loading...

Your Account

Account Home

Checkout   $40.50
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
> Programmable Controllers > Do-more H2 & T1H PLCs (Micro Modular & Stackable)
  •   Shop  
  •   Overview  
  •   In Depth  
Do-more Home Download Free Software
 
Features
Top 11 Ways You Can Do More with this PLC Serial Communications Ethernet Communications High Speed Modules Hign Speed Inputs Motion Control Remote I/O Free Online Training
Free Software
Simulator Auto-Discover I/O Communications Powerful Math Monitoring & Troubleshooting Memory Management Program Management Project Management Security Download the FREE software
Hardware
H2 CPUs T1H CPUs Bases AC I/O Modules DC I/O Modules AC & DC I/O Modules Analog I/O Modules Specialty Modules Go to ZIPLink Selector Tool
Videos


Do-more H2 (Micro Modular PLC) Videos

View Do-more Designer Videos


Detailed Product
Overview



To learn more: https://www.automationdirect.com/do-more?utm_source=RpkBxYy-rys&utm_medium=VideoTeamDescription - (VID-DH-0002)

How to use the Do-more PLC and Do-more Designer Software in a Directlogic PLC System - Overview of the features and benefits of using the Do-more PLC in a Direct Logic 205 PLC system
**The BX-DM1-START, BX-DM1E-START and H2-DM1E-START starter kits are no longer sold.

Online Support Page: https://community.automationdirect.com/s/?utm_source=RpkBxYy-rys&utm_medium=VideoTeamDescription

**Please check our website for our most up-to-date product pricing and availability.


Hide Transcript
View Transcript
If you are already familiar with the Directlogic

205 PLC system, the Do-more CPU is a complete no-brainer. Just swap out the CPU module with the new

Do-more CPU and in addition to retaining almost all of the current 205 functionality, you

instantly get - four times the ladder logic memory,

- 18 times the user data memory - 256 times as many counters

- 256 times as many timers - Over 125 times the number of PID loops

- A possible 20x improvement in scan time - A built-in USB programming port

- And there’s even a version with a built in Ethernet port. All for a price that’s actually lower than

the top of the line direct logic 260 CPU. And if you compare the Do-more with the built

in Ethernet port to that same 260 plus an Ethernet module, well like we said – it’s

a no-brainer. While there is a free version of the DirectSOFT

programming software, it limits you to a hundred words of ladder logic. The fully functional Do-more Designer software

is 100% free. You can download it right now and be up and

running in minutes without hardware because it also has a fully functional built in Do-more

simulator. You can’t use DirectLogic programs on the

new Do-more. It’s a completely different animal inside. Kinda like you can’t run Mac software natively

on a Windows PC. But, the good news is the new Do-more Designer

software took the time-proven DirectSOFT programming software as a starting point, and then took

all of the feedback we’ve gotten from users like you over the years and completely re-worked

it for the best programming experience yet. Check out the Do-more Designer software overview

videos to learn how all those new features will make your life MUCH easier. Speaking of Videos, there are several How

To videos that will walk you through some simple projects so you can see how it all

fits together. Each one is only a couple minutes long so

you get up and running quickly. And the best news is you get FREE on-line

training from Interconnecting Automation with the purchase of every Do-more CPU. Just enter the special code you get with the

Do-more CPU and you will have unlimited access for 30 days. Now I can’t guarantee this offer will last

forever, so take advantage of it today before it goes away. By the way, if you don’t have a DirectLogic

205 PLC system laying around that you can use to test the Do-more CPU, Checkout the

new Do-more Starter kit. It has everything you need to get started. The Do-more Designer Programming Software,

the free training offer, the USB programming cable, a fully populated 3-slot base with

the Do-more CPU and a printed version of the manual. The 205 base is even pre-wired so all you

have to do is plug it in and go. And remember, the Do-more also comes with

the standard AutomationDirect 30 day return policy. Try it. If you don’t like it, just send it back. So why not try it today? Spend Less. Do More. From AutomationDirect.


Playlist Not Found Could not find playlist PLPdypWXY_ROoEcDCcD10Qdb3S9tOmfEn5

Playlist Not Found Could not find playlist PLPdypWXY_ROoJx-HnK9gj2Z5a-i7th-UK

Playlist Not Found Could not find playlist PLPdypWXY_ROqvbaYVBWc3kH-pP01fI4-E

Playlist Not Found Could not find playlist PLPdypWXY_ROr5OPw3e0o8rLC0JQijmCNY

Playlist Not Found Could not find playlist PLPdypWXY_ROrtSkGYNq8Xc52QWTCWf2Ci

Playlist Not Found Could not find playlist PLPdypWXY_ROrRJ5YuFYxs3mSXr9250AN7

Playlist Not Found Could not find playlist PLPdypWXY_ROqJO86ikigKmjnSkbguBKBw

Playlist Not Found Could not find playlist PLPdypWXY_ROqWWy8OnWGt3YD4Dald6uf-

Playlist Not Found Could not find playlist PLPdypWXY_ROrmjIdXLaeovoTLZP65hdac

Playlist Not Found Could not find playlist PLPdypWXY_ROoqTZihvX8c8UUj5GzVCuKH

Playlist Not Found Could not find playlist PLPdypWXY_ROr0ZfCV-fAgau5yDemA19CV

BRX Do-more PLCs - Motion Control & High Speed Inputs
  • Video
    BRX Do-more CTRIO2 Motion Demo Hardware from AutomationDirect
  • Video
    BRX Do-more CTRIO2 Motion Config & JOG from AutomationDirect
  • Video
    BRX Do-more CTRIO2 Motion Dynamic Motion from AutomationDirect
  • Video
    BRX Do-more CTRIO2 Motion Using Limits from AutomationDirect
  • Video
    BRX Do-more CTRIO2 Motion Trapezoid Moves from AutomationDirect
  • Video
    BRX Do-more CTRIO2 Motion Using Encoders from AutomationDirect
BRX Do-more PLCs - Hardware
  • Video
    How To Sense Temperature with a Do-more PLC from AutomationDirect
  • Video
    How To Detect Objects with an AutomationDirect Do-more PLC
  • Video
    AC Motor On/Off with Do-more PLC Part 1 from AutomationDirect
  • Video
    AC Motor On/Off with Do-more PLC Part 2 from AutomationDirect
  • Video
    How to Sense Distance with an AutomationDirect Do-more PLC