AutomationDirect
Search
Login | Register
Accounts & Orders
Cart
1
$40.50

Recent Orders

View and Manage | Request Cancellation
Loading Order History
Loading...Loading...

Your Account

Account Home

Checkout   $40.50
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
> Programmable Controllers > Do-more H2 & T1H PLCs (Micro Modular & Stackable)
  •   Shop  
  •   Overview  
  •   In Depth  
Do-more Home Download Free Software
 
Features
Top 11 Ways You Can Do More with this PLC Serial Communications Ethernet Communications High Speed Modules Hign Speed Inputs Motion Control Remote I/O Free Online Training
Free Software
Simulator Auto-Discover I/O Communications Powerful Math Monitoring & Troubleshooting Memory Management Program Management Project Management Security Download the FREE software
Hardware
H2 CPUs T1H CPUs Bases AC I/O Modules DC I/O Modules AC & DC I/O Modules Analog I/O Modules Specialty Modules Go to ZIPLink Selector Tool
Videos


Do-more H2 (Micro Modular PLC) Videos

View Do-more Designer Videos


Detailed Product
Overview



To learn more: https://www.automationdirect.com/do-more?utm_source=_NoMHDMfZ7Q&utm_medium=VideoTeamDescription - (VID-DM-0028)

Learn how to use a BRX or Do-more PLC to communicate with an Allen Bradley PowerFlex 40 Variable Frequency Drive in this brief tutorial.
**Software Version used in this video: Do-more Designer 1.4.3

Online Support Page: https://community.automationdirect.com/s/?utm_source=_NoMHDMfZ7Q&utm_medium=VideoTeamDescription

**Please check our website for our most up-to-date product pricing and availability.


Hide Transcript
View Transcript
In the Explicit Un-Connected primer video

we saw that EtherNet/IP is really just a bunch lookup tables the device vendor fills out. The blank table template in each class is

called an object and a filled-in table is one specific instance of that object. There was also a table of services – things

you can do with these tables - like get and set the values and another table that listed

the attributes of the whole group – things like how many total instances are there in

the group. All these things taken together are what we

call the Class. Once you have that picture in your mind, getting

or setting a parameter of a EtherNet/IP device is easy. Let’s do a few examples with an Allen Bradley

Power Flex 40 as the server and a Do-more PLC as the Client. In the Do-more Designer software, that Flex

Drive is just another device so as always, we start with system configuration and work

our way down this list. There’s nothing to do at the CPU level,

It doesn’t affect the I/O of the PLC, It’s not a new module, but it is a new device so

we’ll start here. Could we use this one generic EtherNet IP

built-in device to talk to all of our EtherNet/IP hardware? Sure. BUT, it’s better to create a new Do-more

device for each piece of Ethernet IP hardware because each one needs its own TCP/IP connection. If you run all of those through the one generic

EtherNet/IP device, it has to manage all of those which slows things down. If each piece of EtherNet/IP hardware has

its own device, then things get real simple and much faster. So we’ll create a new EthernNet/IP device

for this Flex Drive. New Device, EtherNet/IP Client, OK. Give it a name, how abut FlexDrive and the

rest of this looks fine. That’s it. We just created a device we can talk to. There is no associated I/O mapping and no

new structure because there is nothing for us to interact with in this EtherNet/IP client. Notice that there IS a structure for the EtherNet/IP

SERVER – some people call that the slave – we’ll see that in action in the video

where we use the Do-more as a server to another device. For this video, the Do-more is the Client

or Master device. Great, we’ve created our EtherNet/IP device. Let’s talk to it. In this setup we have a Do-more at this IP

address, a Stride Ethernet switch here and the Allen Bradley PowerFlex40 drive here on

the same subnet at this IP address. To talk to it we just drag the EtherNet/IP

instruction from the toolbox in the Protocol section and fill in the blanks. We want to talk to our PowerFlex device. Remember, that device – which is a lot like

the drivers you have on your windows pc – manages the hardware for you. It takes care of all the handshaking, error

checking, the memory allocation, etc. so you don’t have to mess with any of that. It makes your life easy. We’ll enter the device’s IP address is

this. We have a direct connection so the default

port number is fine. For the rest of this, we just look up the

answers in the PowerFlex 40’s EtherNet/IP Adapter Manual. In Appendix C we see all the different classes

available. We want the Parameter Class so we’ll scroll

down to page C-9. Here’s everything we need to know about

how the parameter information is organized. The Class number is 15. That goes here. This chart is telling me that the Drive Parameters

Numbers ARE the Instance numbers. That means these instance tables we need have

the same numbers as the drive’s parameters – that’s really convenient. In this example we want the nameplate voltage

which is drive parameter 31, so that’s also table - or “instance” - 31. It’s also telling us that instance zero

is the class attribute table – this guy – and here’s the format of that table. So if we wanted to know how many parameters

are in this Class, we would just specify Instance zero, attribute 2. Here’s the object template – the table

format for these instances - the parameter value, name, units, data type, min value,

max value – everything we could want to know about each drive parameter. We want the value of the name plate voltage

for this first example – that’s attribute number 1 - so that number 1 goes here. This is the format for the services table

format for this class. We want to get a single attribute which is

a 0E hex or 14 decimal, so we put that one here. So that’s all there is to it – you just

go to the hardware manual, look up the numbers for the service, Class, Instance, and the

attribute of that instance that you want and you’re done. In this example we want to get from the parameter

class, parameter 31 which is instance 31 – and we want to know the nameplate voltage of that

instance which is attribute number 1. We’ll enable this on an edge, set these

bits on success and error and put the response here which I happen to know is a 16 bit unsigned

result – I’ll show you how I know that in just a minute – which is 2 bytes max. Let’s add a control bit so we can enable

this instruction and transfer the project …

Let’s bring up a data view and monitor the result which we put in D1 and the result length

which we put in D2. Let’s also add the control bit so we can

activate the instruction. When I toggle that control bit, I see the

request was successful and the name plate voltage is 225 Volts and that two bytes were

returned. Perfect. That’s all there is to it. Given these tables, we just look up what we

want and fill in the blanks. EtherNet/IP is easy once you understand how

to navigate these tables. How did I know that the nameplate voltage

was an unsigned 16 bit integer? I ask asked for it! You can see back in appendix C that the data

type is attribute number 5. Let’s try that. And since it’s almost the exact same thing

as we just did, let’s just copy that instruction and modify it. The only thing we need to change is the attribute

we want – instead of the parameter value we want the data type which is number 5. And let’s put that result in D3 and the

length in D4. And let’s use these as our success bits. We see in appendix C, attribute number 5,

is an unsigned integer or 8 bits, so we only need one byte for that. Click OK. Let’s trigger this instruction on the success

of the previous one. And write it out to the Do-more. And over in the Data view let’s add our

new results. Toggle the control bit and sure enough, the

device tells us the data type for parameter 31 is 199 which is C7 hex which according

to our lookup table is Unsigned 16 bit. So before I started this video, I executed

this command so I would know the data type to use for that first example we did. Again, everything you need to know is in these

tables and once you understand how to use them you will be in total control of your

device. Let’s do another one. Let’s get the name of this parameter. Again, it’s almost identical to what we

just did, so we’ll just copy this instruction. Same Class – or group of tables. Same Instance – or table number. The only difference is now we want a different

row of the table – or attribute of the parameter. We see back in appendix C that the name of

the parameter is attribute 7 and that it is a short string. So we put a 7 here, and put the result in

a string structure. Change the success bits and we’re Done. Trigger this one on the success of the previous

one. Accept everything, and write out to the Do-more. Add the string to the data view, toggle the

control bit and we see the name of this parameter is “Motor Name Plate Voltage.” Awesome. Do you notice this little dot here? That’s because the string sent to us from

the flex drive has a leading length byte. If I switch this to Hex display this 10 hex

which is 16 decimal is a count of the characters in the string. And if we do a short string zero dot length

– it agrees – there are a total of 17 characters – which includes the length byte

– in this string. Perfect. Ok, this time we’re going to ask the Flex

Drive what the units of the Name Plate Voltage are. It’s exactly what we just did so we’ll

copy that instruction and change the attribute we want to the Units Attribute, attribute

number 8. Change the status bits, put the result in

short string 1. Great. Let’s enable this instruction on successful

completion of the parameter name request. Accept the changes and write the project to

the Do-more. And I’ll add the units string to our dataview. Toggle the initial name plate voltage control

bit, and sure enough, we see the units are volts. What if we wanted to do all of this for the

acceleration parameter? Same thing, Right? Except now we want parameter or “instance”

number 39. What if you wanted to set a parameter instead

of get one? Well, the SET service code is 10 hex or 16

decimal. Everything else is pretty much the same. As you can see, once you get the hang of using

these groups of tables – or “Classes” – it’s easy to get or set anything you

want using just the one explicit message instruction. And keep in mind – we only messed with the

Parameter class of this device – there are a bunch of others you can explore simply by

changing the class number here. The only hard part of all of this is finding

the documents that have the EtherNet/IP class information – you know, all those filled

out tables - for your target device. Once you’ve done that, the rest is easy. If you have any questions, please contact

AutomationDirect’s FREE award winning tech support during regular business hours – they

will be happy to help you with any AutomationDirect parts. The PowerFlex drive isn’t an AutomationDirect

part so don’t ask them about that, but you can ask folks on the forums – they love

to share their years of experience! Just don’t post any questions directed at

AutomationDIrect’s support staff there, they don’t monitor the forums on a regular

basis. Spend Less, Do More. With AutomationDirect.


Playlist Not Found Could not find playlist PLPdypWXY_ROoEcDCcD10Qdb3S9tOmfEn5

Playlist Not Found Could not find playlist PLPdypWXY_ROoJx-HnK9gj2Z5a-i7th-UK

Playlist Not Found Could not find playlist PLPdypWXY_ROqvbaYVBWc3kH-pP01fI4-E

Playlist Not Found Could not find playlist PLPdypWXY_ROr5OPw3e0o8rLC0JQijmCNY

Playlist Not Found Could not find playlist PLPdypWXY_ROrtSkGYNq8Xc52QWTCWf2Ci

Playlist Not Found Could not find playlist PLPdypWXY_ROrRJ5YuFYxs3mSXr9250AN7

Playlist Not Found Could not find playlist PLPdypWXY_ROqJO86ikigKmjnSkbguBKBw

Playlist Not Found Could not find playlist PLPdypWXY_ROqWWy8OnWGt3YD4Dald6uf-

Playlist Not Found Could not find playlist PLPdypWXY_ROrmjIdXLaeovoTLZP65hdac

Playlist Not Found Could not find playlist PLPdypWXY_ROoqTZihvX8c8UUj5GzVCuKH

Playlist Not Found Could not find playlist PLPdypWXY_ROr0ZfCV-fAgau5yDemA19CV

BRX Do-more PLCs - Motion Control & High Speed Inputs
  • Video
    BRX Do-more CTRIO2 Motion Demo Hardware from AutomationDirect
  • Video
    BRX Do-more CTRIO2 Motion Config & JOG from AutomationDirect
  • Video
    BRX Do-more CTRIO2 Motion Dynamic Motion from AutomationDirect
  • Video
    BRX Do-more CTRIO2 Motion Using Limits from AutomationDirect
  • Video
    BRX Do-more CTRIO2 Motion Trapezoid Moves from AutomationDirect
  • Video
    BRX Do-more CTRIO2 Motion Using Encoders from AutomationDirect
BRX Do-more PLCs - Hardware
  • Video
    How To Sense Temperature with a Do-more PLC from AutomationDirect
  • Video
    How To Detect Objects with an AutomationDirect Do-more PLC
  • Video
    AC Motor On/Off with Do-more PLC Part 1 from AutomationDirect
  • Video
    AC Motor On/Off with Do-more PLC Part 2 from AutomationDirect
  • Video
    How to Sense Distance with an AutomationDirect Do-more PLC