> Programmable Controllers > Do-more H2 & T1H PLCs (Micro Modular & Stackable)
  •   Shop  
  •   Overview  
  •   In Depth  
Do-more Home Download Free Software
 
Features
Top 11 Ways You Can Do More with this PLC Serial Communications Ethernet Communications High Speed Modules Hign Speed Inputs Motion Control Remote I/O Free Online Training
Free Software
Simulator Auto-Discover I/O Communications Powerful Math Monitoring & Troubleshooting Memory Management Program Management Project Management Security Download the FREE software
Hardware
H2 CPUs T1H CPUs Bases AC I/O Modules DC I/O Modules AC & DC I/O Modules Analog I/O Modules Specialty Modules Go to ZIPLink Selector Tool
Videos


Do-more H2 (Micro Modular PLC) Videos

View Do-more Designer Videos


Detailed Product
Overview



To learn more: https://www.automationdirect.com/plcs?utm_source=bOnEKXDBt8A&utm_medium=VideoTeamDescription - (VID-DH-0001)

The BRX Do-more Series PLC is the next generation programmable controller built on a strong PLC foundation that makes control applications easier to implement. Do-more uses proven DirectLOGIC DL205 hardware for a flexible control platform and introduces a powerful, intuitive set of new programming tools. This combination of Do-more H2 Series CPUs and the existing line of AutomationDirect 205 series I/O modules and base units creates an incredibly powerful micro modular PLC at a fraction of the cost of comparable PLCs.
**The BX-DM1-START, BX-DM1E-START and H2-DM1E-START starter kits are no longer sold.

Online Support Page: https://community.automationdirect.com/s/?utm_source=bOnEKXDBt8A&utm_medium=VideoTeamDescription

**Please check our website for our most up-to-date product pricing and availability.


Hide Transcript
View Transcript
Welcome to Kickstart where you get to see

new products here at AutomationDirect. I am excited to show you our newest PLC Controller

for the DL205 series called: Do More! This new PLC line offers features and performance

of high-end PLCs for an economical price. Using the proven DirectLOGIC DL205 hardware

as a platform, the Do-more H2 PLC supports all base units, discrete and analog I/O modules

available for the DL205 PLC. Do more CPU modules are avail with and without

Ethernet built in, enabling you to save cost and rack space by utilizing the H2-DM1E with

Ethernet. Both modules have a USB port which makes connectivity

to the Do more designer software a breeze. We also offer Do more as a starter kit that

includes hardware, programming cable, user manual, software CD, and a 30 day free access

to online video training. Do More has a much more flexible and advanced

design that makes integrating I/O and organizing a program much easier. The H2 CPUs offer four times more program

memory, nine times more data memory, and operate at speeds up to 20 times faster than current

DL205 CPUs. With a wide array of high-level program blocks

in Do-more, developers can use two or three instructions to program functionality that

used to require many lines of hard-to-understand ladder logic. Do-more provides an advanced instruction set

to reduce programming time, superior memory mapping to improve data management, and data

structures to simplify initial programming and long-term software maintenance. Do More is Stage based programming which can

be better at controlling sequential process like machine control. Do more supports Axis mode instructions that

offer a more dynamic way of commanding motion through our H2-CTRIO2 module. It offers tools like: stepping through program,

force stages on and off and more. Do More provides a list of devices in the

system with their status. The user documentation like nicknames, rung

comments etc are all stored on the CPU. Multiple passwords, up to 256 user programs,

run time editing, over 2000 PID loops! And, memory back up is included. WOW!! And….the Do-more Designer software can be

downloaded free of charge. Do More was designed and built by our long

time friends at HOST engineering. You can find the agency approvals and specs

for the Do More products on our website at : www.automationdirect.com Don’t forget to check out all of our programmable

controller lines from micro to bricks to modular and specialty PLCs all the way up to PACs…

and you can find them all right here at automationdirect. Check back with us often on AutomationDirects

websites or on Youtube.com/Automationdirect for more Kickstart videos. If you are watching us on YouTube, please

let us know what you think about the products or how you plan to use them in your application

by leaving us a comment down below. Thanks for watching and we hope to see you

again soon.


Playlist Not Found Could not find playlist PLPdypWXY_ROoEcDCcD10Qdb3S9tOmfEn5

Playlist Not Found Could not find playlist PLPdypWXY_ROoJx-HnK9gj2Z5a-i7th-UK

Playlist Not Found Could not find playlist PLPdypWXY_ROqvbaYVBWc3kH-pP01fI4-E

Playlist Not Found Could not find playlist PLPdypWXY_ROr5OPw3e0o8rLC0JQijmCNY

Playlist Not Found Could not find playlist PLPdypWXY_ROrtSkGYNq8Xc52QWTCWf2Ci

Playlist Not Found Could not find playlist PLPdypWXY_ROrRJ5YuFYxs3mSXr9250AN7

Playlist Not Found Could not find playlist PLPdypWXY_ROqJO86ikigKmjnSkbguBKBw

Playlist Not Found Could not find playlist PLPdypWXY_ROqWWy8OnWGt3YD4Dald6uf-

Playlist Not Found Could not find playlist PLPdypWXY_ROrmjIdXLaeovoTLZP65hdac

Playlist Not Found Could not find playlist PLPdypWXY_ROoqTZihvX8c8UUj5GzVCuKH

Playlist Not Found Could not find playlist PLPdypWXY_ROr0ZfCV-fAgau5yDemA19CV

BRX Do-more PLCs - Motion Control & High Speed Inputs
  • Video
    BRX Do-more CTRIO2 Motion Demo Hardware from AutomationDirect
  • Video
    BRX Do-more CTRIO2 Motion Config & JOG from AutomationDirect
  • Video
    BRX Do-more CTRIO2 Motion Dynamic Motion from AutomationDirect
  • Video
    BRX Do-more CTRIO2 Motion Using Limits from AutomationDirect
  • Video
    BRX Do-more CTRIO2 Motion Trapezoid Moves from AutomationDirect
  • Video
    BRX Do-more CTRIO2 Motion Using Encoders from AutomationDirect
BRX Do-more PLCs - Hardware
  • Video
    How To Sense Temperature with a Do-more PLC from AutomationDirect
  • Video
    How To Detect Objects with an AutomationDirect Do-more PLC
  • Video
    AC Motor On/Off with Do-more PLC Part 1 from AutomationDirect
  • Video
    AC Motor On/Off with Do-more PLC Part 2 from AutomationDirect
  • Video
    How to Sense Distance with an AutomationDirect Do-more PLC