> Programmable Controllers > Do-more H2 & T1H PLCs (Micro Modular & Stackable)
  •   Shop  
  •   Overview  
  •   In Depth  
Do-more Home Download Free Software
 
Features
Top 11 Ways You Can Do More with this PLC Serial Communications Ethernet Communications High Speed Modules Hign Speed Inputs Motion Control Remote I/O Free Online Training
Free Software
Simulator Auto-Discover I/O Communications Powerful Math Monitoring & Troubleshooting Memory Management Program Management Project Management Security Download the FREE software
Hardware
H2 CPUs T1H CPUs Bases AC I/O Modules DC I/O Modules AC & DC I/O Modules Analog I/O Modules Specialty Modules Go to ZIPLink Selector Tool
Videos


Do-more H2 (Micro Modular PLC) Videos

View Do-more Designer Videos


Detailed Product
Overview



To learn more: https://www.automationdirect.com/do-more?utm_source=dE66Jp9ADM8&utm_medium=VideoTeamDescription - (VID-DM-0032)

Learn how to use an EtherNet/IP Explicit Do-more PLC client with an AutomationDirect SR55 Soft Starter in this brief tutorial.
**Software Version used in this video: Do-more Designer 1.4.3

Online Support Page: https://community.automationdirect.com/s/?utm_source=dE66Jp9ADM8&utm_medium=VideoTeamDescription

**Please check our website for our most up-to-date product pricing and availability.


Hide Transcript
View Transcript
Controlling the SR55 Soft Starter via EtherNet/IP

Explicit Messaging is easy with the Do-more. If you go to the SR55 product page on the

AutomationDirect website and click on the User Manual, you will see a section dedicated

to communications. Looks like EtherNet/IP coverage starts on

page 5-9. The first thing you see is a list of all the

things you can monitor and control on the SR55 Soft Starter via EtherNet/IP. The first thing you’ll need to do is get

the IP Configuration Tool so you can set the IP Address of the unit. There’s a link in the user manual that will

take you to this page. Download and install this utility. It’s small and will download quickly. The user manual tells you how to handle window

8, we’re using 7 here so we can skip that. Note that the user guide encourages you to

connect to the SR55 directly through a switch or a crossover cable and to make sure there

is nothing else on the network. Press scan to find your soft starter. If you don’t get anything and you have multiple

Ethernet adapters in your PC you can tell the utility exactly which adapter your starter

is connected to here. Once you find the drive, double click on it

to change the address. There is a DCHP option, but it is rare that

you would want to use that. Hit set, and sure enough we see the new IP

Address. Power cycle the drive to get the new setting

to show up on the starter’s touch screen. Home, Device, go to the next screen and press

Networks. There’s our EtherNet/IP network and it’s

parameters with our new IP Address. Perfect. We’re ready to talk to the drive via EtherNet/IP. Over on the Do-more I setup a new project

and connected to my Do-more and made sure the Do-more’s IP Address was in the same

sub-domain as the SR55 Soft Starter. We always start a Do-more project by working

our way down the system configuration list. The Do-more is a client making requests of

the SR55 soft starter which is the server, so we don’t need to setup a server on the

Do-more. There’s no new I/O configuration since we’re

using the Ethernet port, and we’re not adding any modules. We are talking to a new device and while we

could use the built-in EtherNet/IP device for this, it is alwyas better to get in the

habit of creating a new Do-more Device for each new piece of hardware – that’s so

the Do-more device doesn’t have to manage multiple TCP/IP connections which can slow

down your code. So we’ll create a New, EtherNet/IP device,

and we’ll call it Soft Starter. Great, we now have a Do-more Deice that will

manage the hardware for us. We just talk to it and it handles all the

low level messaging, buffer management, handshaking, and timing, etc. for us. I love that. We didn’t add any I/O to the system and

since we didn’t create a new heap item, there’s nothing to look at in the memory

configuration. We’re done with setting up the Do-more. To talk to the Soft Starter via Explicit EtherNet/IP

messaging, we just drop an Explicit messaging instruction on a rung and fill in the blanks. We want to use the new Soft Starter Do-more

Device we just created and the Soft Starter is at this IP address. This is where we put the codes we send to

the Soft Starter. Page 5-17 of the soft starter user manual

has a chart that shows us all the code we need. First , to run the starter via EtherNet/IP

you have to set this Network control bit to a one. So we just copy these numbers over to here,

class 41, instance 1, attribute 5 and we want to set that on the starter. Let’s trigger this instruction from our

ladder code and we’ll want to use these control bits for status. Let’s use D0 so we can change the Ethernet

Enable during run-time if we want to and we only need to send one bit, so we only need

one byte. Accept that. Let’s trigger this on C101. I’m using a rising edge contact here. Did I need to do that? No. We told the instruction to only execute on

the leading edge, but I like to do it here just to remind myself that was the intent. This little triangle also reminds me this

instruction is triggered on an edge. Let’s add another instruction to RUN the

starter. It’s the exact same thing so I’ll just

copy this instruction and paste it down here. The only difference is we want to write to

attribute 3 now. We’ll also use different status bits and

we’ll use D1 for our data register. Let’s trigger this on C102. Again I don’t have to use a rising edge

contact here – it’s just the way I like to do it. Well, let’s accept everything write it out

to the Do-more. Let’s bring up a Dataview and add the control

bits and the results registers. Make sure we’re running. Turn on edit mode and write a 1 to D0 and

toggle that control bit to enable Ethernet communications. Now let’s try and start the drive. We’ll put a 1 in D1 and toggle that instruction. Sure enough the starter tries to start but

then it faults out because we don’t have a motor connected. Let’s add an instruction to clear the fault. It’s nearly identical to this one, we’ll

just copy that, and paste it here and double click to edit. Looks like fault reset is attribute 12 – that

goes here - and we’ll use different status bits and we’ll use D2 for the value to send

- which will be a one for reset. And let’s add contact 103 to trigger that

instruction. Ok, accept all of that and write it out to

the Do-more. Add the new contact and memory locations to

the data view and make sure we’re running. Let’s clear the run bit and write that out

so the motor won’t try and start running again once we clear the fault. To clear the fault we put a 1 in here and

then toggle the instruction. Sure enough, the drive is reset and ready

to go. So using Explicit messaging with the Do-more

PLC and the AutomationDirect SR55 Soft Starter is pretty easy. Just look up what you want in this table in

the user manual and use it to fill in the blanks in the Explicit Ethernet/IP instruction. If you need any help, contact AutomationDirect’s

Free Award Winning Tech Support during regular business hours – they will be happy to help

you. And don’t forget the forums. There are lots of folks there that love to

share their years of experience. Just don’t post any questions directed at

AutomationDirect’s support staff there – they don’t monitor the forums on a regular basis. Spend Less

Do-more With Automation Direct.


Playlist Not Found Could not find playlist PLPdypWXY_ROoEcDCcD10Qdb3S9tOmfEn5

Playlist Not Found Could not find playlist PLPdypWXY_ROoJx-HnK9gj2Z5a-i7th-UK

Playlist Not Found Could not find playlist PLPdypWXY_ROqvbaYVBWc3kH-pP01fI4-E

Playlist Not Found Could not find playlist PLPdypWXY_ROr5OPw3e0o8rLC0JQijmCNY

Playlist Not Found Could not find playlist PLPdypWXY_ROrtSkGYNq8Xc52QWTCWf2Ci

Playlist Not Found Could not find playlist PLPdypWXY_ROrRJ5YuFYxs3mSXr9250AN7

Playlist Not Found Could not find playlist PLPdypWXY_ROqJO86ikigKmjnSkbguBKBw

Playlist Not Found Could not find playlist PLPdypWXY_ROqWWy8OnWGt3YD4Dald6uf-

Playlist Not Found Could not find playlist PLPdypWXY_ROrmjIdXLaeovoTLZP65hdac

Playlist Not Found Could not find playlist PLPdypWXY_ROoqTZihvX8c8UUj5GzVCuKH

Playlist Not Found Could not find playlist PLPdypWXY_ROr0ZfCV-fAgau5yDemA19CV

BRX Do-more PLCs - Motion Control & High Speed Inputs
  • Video
    BRX Do-more CTRIO2 Motion Demo Hardware from AutomationDirect
  • Video
    BRX Do-more CTRIO2 Motion Config & JOG from AutomationDirect
  • Video
    BRX Do-more CTRIO2 Motion Dynamic Motion from AutomationDirect
  • Video
    BRX Do-more CTRIO2 Motion Using Limits from AutomationDirect
  • Video
    BRX Do-more CTRIO2 Motion Trapezoid Moves from AutomationDirect
  • Video
    BRX Do-more CTRIO2 Motion Using Encoders from AutomationDirect
BRX Do-more PLCs - Hardware
  • Video
    How To Sense Temperature with a Do-more PLC from AutomationDirect
  • Video
    How To Detect Objects with an AutomationDirect Do-more PLC
  • Video
    AC Motor On/Off with Do-more PLC Part 1 from AutomationDirect
  • Video
    AC Motor On/Off with Do-more PLC Part 2 from AutomationDirect
  • Video
    How to Sense Distance with an AutomationDirect Do-more PLC