> Programmable Controllers > Do-more H2 & T1H PLCs (Micro Modular & Stackable)
  •   Shop  
  •   Overview  
  •   In Depth  
Do-more Home Download Free Software
 
Features
Top 11 Ways You Can Do More with this PLC Serial Communications Ethernet Communications High Speed Modules Hign Speed Inputs Motion Control Remote I/O Free Online Training
Free Software
Simulator Auto-Discover I/O Communications Powerful Math Monitoring & Troubleshooting Memory Management Program Management Project Management Security Download the FREE software
Hardware
H2 CPUs T1H CPUs Bases AC I/O Modules DC I/O Modules AC & DC I/O Modules Analog I/O Modules Specialty Modules Go to ZIPLink Selector Tool
Videos


Do-more H2 (Micro Modular PLC) Videos

View Do-more Designer Videos


Detailed Product
Overview



To learn more: https://www.automationdirect.com/do-more?utm_source=aWebmMTRcFw&utm_medium=VideoTeamDescription - (VID-DM-0021)

This video covers step by step instructions on how to setup and use a C-more HMI display with the BRX Do-more PLCs so the C-more can access all of the Do-more memory.

Online Support Page: https://community.automationdirect.com/s/?utm_source=aWebmMTRcFw&utm_medium=VideoTeamDescription

**Please check our website for our most up-to-date product pricing and availability.


Hide Transcript
View Transcript
Connecting a C-more HMI to a DoMore can be

done via the typical Modbus route. When you create the TAGs in the C-more, you’ll

just have the usual four options and those four options will correspond to the 4 memory

areas reserved for Modbus commands in the Do-more right here. The Do-more can then use those to control

IO or anything else you want. That will work just fine. OR you can do it the EASY way. All you have to do is specify the DoMore protocol

in your C-more more project. And all of the sudden the C-more has full

access to ALL of these memory areas in the DoMore. Let’s take a look. When you create a new C-more project, You

give it a name, select the panel you are using – I’m using this guy right here - and

then right here, just select the AutomationDirect DoMore protocol – I’m using Ethernet,

so I’ll select that one. You can do the Protocol setup right here,

but I prefer to do it over here in the panel manager. In the Panel manager, I just select the device

I want to talk to, and fill in the Protocol. The nice thing about doing it here though,

is I can change the name of the device. We just enter the IP address of this DoMore

and a password if you’re DoMore is setup to use one. Mine doesn’t so I’ll leave it blank. If we had chosen the serial version of this

protocol you would be filling in baud rate, stop bits, parity, etc. Well, that’s all there is to it. Just enter the IP address, give your device

a name, say OK That was setting up the Do-more in our C-more

project. now we need to setup the panels networking

information. Under the Ethernet port tab we put in the

panels IP Address and enter a subnet mask. So again, to set this up all we had to do

was: 1. Setup the DoMore device under the panel manager,

2. And setup the panels networking under the

touch panel network. That’s it, now everything becomes real easy

because when I create a TAG to talk to the DoMore, I just select the Do-more device,

Give it a name – let’s have this TAG control – oh I don’t know – how about output

Y0. I’ll call it Out Y0. That’s going to be a discrete, and when

I select that, it automatically selects all of the memory areas in the Do-more that are

a discrete data type. In this case, I want the Y’s. And I want to modify Y0. That’s it. And while we are at it, let’s go ahead and

control an analog output. That will be a signed 16 bit integer, and

once I have selected that, the C-more automatically populates all the available memory areas in

the Do-more. In this case, we want the analog Y out at

address 0. Let’s add a pushbutton to drive that Y0

output we created. And let’s add an increment decrement to

drive that analog output. Let’s transfer that to the panel I have

here on my desk. Here is a new online DoMore project. You setup the Ethernet connection right here

under the info button: Set node and IP configuration. In this example, I have already setup our

Do-more for this IP address and this subnet mask. Now we’ll just save and download this to

the DoMore. And we are up and running. Note that we didn’t enter any ladder code. If I bring up a DataView to monitor those

TAGs we created – one was driving Y0 and one was driving the analog Y0 – and I reach

over to my panel and I press the OFF button, sure enough – Y0 toggles on the Do-more. Likewise, if I hit the increment button, I

can see my analog value changing. Again, without any effort on the part of the

Do-more – it just works. So because we selected that Do-more driver

in the C-more application, the C-more now has full access to all the memory areas in

the DoMore, the DoMore doesn’t really have to do anything. All the data just ends up where it is supposed

to ready for the DoMore to use it whoever it wants. Here’s the hardware setup we used in this

example: The C-More is connected to the DoMore via

Ethernet – note you need a crossover cable to do this – and the PC is connected to

the C-More and the Do-more via USB. Be sure to check out the other videos in this

series for more ways to get up and running quickly with the DoMore PLC Spend Less. Do More. From Automation Direct.


Playlist Not Found Could not find playlist PLPdypWXY_ROoEcDCcD10Qdb3S9tOmfEn5

Playlist Not Found Could not find playlist PLPdypWXY_ROoJx-HnK9gj2Z5a-i7th-UK

Playlist Not Found Could not find playlist PLPdypWXY_ROqvbaYVBWc3kH-pP01fI4-E

Playlist Not Found Could not find playlist PLPdypWXY_ROr5OPw3e0o8rLC0JQijmCNY

Playlist Not Found Could not find playlist PLPdypWXY_ROrtSkGYNq8Xc52QWTCWf2Ci

Playlist Not Found Could not find playlist PLPdypWXY_ROrRJ5YuFYxs3mSXr9250AN7

Playlist Not Found Could not find playlist PLPdypWXY_ROqJO86ikigKmjnSkbguBKBw

Playlist Not Found Could not find playlist PLPdypWXY_ROqWWy8OnWGt3YD4Dald6uf-

Playlist Not Found Could not find playlist PLPdypWXY_ROrmjIdXLaeovoTLZP65hdac

Playlist Not Found Could not find playlist PLPdypWXY_ROoqTZihvX8c8UUj5GzVCuKH

Playlist Not Found Could not find playlist PLPdypWXY_ROr0ZfCV-fAgau5yDemA19CV

BRX Do-more PLCs - Motion Control & High Speed Inputs
  • Video
    BRX Do-more CTRIO2 Motion Demo Hardware from AutomationDirect
  • Video
    BRX Do-more CTRIO2 Motion Config & JOG from AutomationDirect
  • Video
    BRX Do-more CTRIO2 Motion Dynamic Motion from AutomationDirect
  • Video
    BRX Do-more CTRIO2 Motion Using Limits from AutomationDirect
  • Video
    BRX Do-more CTRIO2 Motion Trapezoid Moves from AutomationDirect
  • Video
    BRX Do-more CTRIO2 Motion Using Encoders from AutomationDirect
BRX Do-more PLCs - Hardware
  • Video
    How To Sense Temperature with a Do-more PLC from AutomationDirect
  • Video
    How To Detect Objects with an AutomationDirect Do-more PLC
  • Video
    AC Motor On/Off with Do-more PLC Part 1 from AutomationDirect
  • Video
    AC Motor On/Off with Do-more PLC Part 2 from AutomationDirect
  • Video
    How to Sense Distance with an AutomationDirect Do-more PLC