> Programmable Controllers > Do-more H2 & T1H PLCs (Micro Modular & Stackable)
  •   Shop  
  •   Overview  
  •   In Depth  
Do-more Home Download Free Software
 
Features
Top 11 Ways You Can Do More with this PLC Serial Communications Ethernet Communications High Speed Modules Hign Speed Inputs Motion Control Remote I/O Free Online Training
Free Software
Simulator Auto-Discover I/O Communications Powerful Math Monitoring & Troubleshooting Memory Management Program Management Project Management Security Download the FREE software
Hardware
H2 CPUs T1H CPUs Bases AC I/O Modules DC I/O Modules AC & DC I/O Modules Analog I/O Modules Specialty Modules Go to ZIPLink Selector Tool
Videos


Do-more H2 (Micro Modular PLC) Videos

View Do-more Designer Videos


Detailed Product
Overview



To learn more: https://www.automationdirect.com/do-more?utm_source=w7Dh2whozRs&utm_medium=VideoTeamDescription - (VID-DM-0037)

A quick programming example so you can see how to 1) Connect to the Do-more BRX PLC via USB, 2) Write a program and 3) Transfer it to the PLC.
**Software Version used in this video: Do-more Designer 2.0

Online Support Page: https://community.automationdirect.com/s/?utm_source=w7Dh2whozRs&utm_medium=VideoTeamDescription

**Please check our website for our most up-to-date product pricing and availability.


Hide Transcript
View Transcript
Plugging a USB cable from your computer into

the Do-more PLC is the easiest way to get started because it doesn’t require any Ethernet

or Serial Port setup. Power up the PLC and you’ll hear the familiar

Windows connected sound. When you start Do-more Designer, you can choose

if you want to work on a previous project, create a new one off line from a PLC or in

our case we want to create a new on-line project. If you have an existing link to a PLC you

can click on it here. We have a new PLC so we’ll click ADD to

create a new link. We’re connected via USB, and Do-more Designer

shows us the one PLC that is connected via USB. Give the new link a name and now we can select

that guy as the PLC we want to work with. We can skip these dialogs for now. Since we’re connected to a Do-more PLC,

we get a dashboard with an image of that PLC, groupings of all the things we can do with

the PLC and hot spots right on the PLC so you can just point and click to configure

whatever part of the PLC you want without having to search through a bunch of menus. We really just want to start writing ladder

code so just click on View/Edit Program. I’ve been using this PLC so let’s reset

it back to factory default. Normally you want to clear everything BUT

the system settings because it has the Ethernet settings you need to communicate with the

PLC, if you are using Ethernet. We’re using USB so it doesn’t matter,

so let’s take it all the way back to factory default. Are we sure? Yep. The clock is fine and we don’t need to change

the system configuration. Great, we now have a clean factory fresh PLC. This little exclamation point is reminding

us that we don’t have a current project in the PLC – we know that – we just cleared

the memory – right? That will go away when we write our first

project. Move the switch to STOP and then to TERM. Great, our systems should be in sync. In ladder programming our goal is to get power

to flow from this power rail, through some controlling logic over to this output column. This hollow cursor reminds me I’m not in

edit mode, so I’ll click on the edit button. The cursor becomes solid and our instruction

toolbox appears. Let’s un-pin that so we have more room to

work. Let’s grab a normally open contact and drop

it on the first rung. Let’s use the X0 input. Ok, let’s grab an output coil and drop it

in the output column. Let’s drive the Y0 output. The yellow bar reminds me that I haven’t

accepted this program yet so I’ll do that. This is kinda like compiling – Do-more designer

checks everything to make sure it is ready to transfer to the PLC. Now I get a green bar which tells me the change

hasn’t been saved and the blue bar which says it hasn’t been written to the PLC yet. Let’s save it – green bar goes away. And let’s write it to the PLC and the blue

bar goes away. Perfect. I see down here that the PLC is in terminal

mode so I’ll reach over and flip its switch to RUN. Now it says the switch is in RUN mode and

that the PLC is in fact running the program. I wired a push button to input X0, so if we

enable status monitoring, and I press that button, sure enough we see output Y0 go active. Exactly what we expected. Well … That’s all there is to connecting

to a PLC via USB, writing a quick program, and transferring it to the PLC. Could you download this program to the built-in

simulator to test it with no hardware? Sure. Go to the start page and click on this button

to search for videos on using the simulator. You can type simulator here, or click the

simulator category and even show all related videos. You can watch that video right now or download

it so you can watch it later off line. And if you need any help with Do-more Designer,

please contact AutomationDirect’s free award winning support team during regular business

hours. They will be happy to help. Spend Less ... Do-more ... with AutomationDirect.


Playlist Not Found Could not find playlist PLPdypWXY_ROoEcDCcD10Qdb3S9tOmfEn5

Playlist Not Found Could not find playlist PLPdypWXY_ROoJx-HnK9gj2Z5a-i7th-UK

Playlist Not Found Could not find playlist PLPdypWXY_ROqvbaYVBWc3kH-pP01fI4-E

Playlist Not Found Could not find playlist PLPdypWXY_ROr5OPw3e0o8rLC0JQijmCNY

Playlist Not Found Could not find playlist PLPdypWXY_ROrtSkGYNq8Xc52QWTCWf2Ci

Playlist Not Found Could not find playlist PLPdypWXY_ROrRJ5YuFYxs3mSXr9250AN7

Playlist Not Found Could not find playlist PLPdypWXY_ROqJO86ikigKmjnSkbguBKBw

Playlist Not Found Could not find playlist PLPdypWXY_ROqWWy8OnWGt3YD4Dald6uf-

Playlist Not Found Could not find playlist PLPdypWXY_ROrmjIdXLaeovoTLZP65hdac

Playlist Not Found Could not find playlist PLPdypWXY_ROoqTZihvX8c8UUj5GzVCuKH

Playlist Not Found Could not find playlist PLPdypWXY_ROr0ZfCV-fAgau5yDemA19CV

BRX Do-more PLCs - Motion Control & High Speed Inputs
  • Video
    BRX Do-more CTRIO2 Motion Demo Hardware from AutomationDirect
  • Video
    BRX Do-more CTRIO2 Motion Config & JOG from AutomationDirect
  • Video
    BRX Do-more CTRIO2 Motion Dynamic Motion from AutomationDirect
  • Video
    BRX Do-more CTRIO2 Motion Using Limits from AutomationDirect
  • Video
    BRX Do-more CTRIO2 Motion Trapezoid Moves from AutomationDirect
  • Video
    BRX Do-more CTRIO2 Motion Using Encoders from AutomationDirect
BRX Do-more PLCs - Hardware
  • Video
    How To Sense Temperature with a Do-more PLC from AutomationDirect
  • Video
    How To Detect Objects with an AutomationDirect Do-more PLC
  • Video
    AC Motor On/Off with Do-more PLC Part 1 from AutomationDirect
  • Video
    AC Motor On/Off with Do-more PLC Part 2 from AutomationDirect
  • Video
    How to Sense Distance with an AutomationDirect Do-more PLC