• Credit Application
  • Tax Exemption
| Direct Sales in US and Canada | 1-800-633-0405 | About Us | Contact Us | Line Card
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
> Programmable Controllers > BRX PLCs (Stackable Micro Brick)
  •   Shop  
  •   Overview  
  •   In Depth  
BRX Home BRX - Your Automation Foundation Configure a BRX
 
Features
10 ways it's better with BRX PLCs! IIoT Edge Device: Your low cost link to Industry 4.0..and beyond! Not Your Everyday Analog Security Simple Data Logging/Advanced Data Control Fortified with American Pride Easy Migration Motion Control/Positioning made easy!
Free Software
What's New with Do-more Designer Dashboard- Easy Navigation Simulator Easy PID Auto-Discover I/O Powerful Math Troublefree Troubleshooting DirectLOGIC Migration Instruction Set Free Online Training Video Help Download the Free Software
Hardware
Hardware Overview M Series CPUs (no I/O) 10-point Series CPUs 18-point Series CPUs 36-point Series CPUs Ethernet Remote I/O Expansion Modules Pluggable Option Modules Connection Options Spare Parts Go to ZIPLink Selector Tool
Videos


BRX Series PLCs (Stackable Micro Brick) Videos

View Do-more Designer Video


Detailed Product
Overview



To learn more: https://www.automationdirect.com/do-more?utm_source=cmSZ5ubh4Ig&utm_medium=VideoTeamDescription - (VID-DM-0040)

A quick spin through the most common BRX Do-more technical questions with links to video tutorials to learn more about each topic. Emphasis on the new Video Search tool included in Do-more Designer 2.0!
** Software Version used in this video: Do-more Designer 2.0

Online Support Page: https://community.automationdirect.com/s/?utm_source=cmSZ5ubh4Ig&utm_medium=VideoTeamDescription

**Please check our website for our most up-to-date product pricing and availability.


Hide Transcript
View Transcript
This is a list of the most common questions

the AutomationDirect support team gets on Do-more PLCs. We thought we would share the answers to hopefully

save you from struggling with them yourself. Number 1: How do I connect my computer to

my Do-more PLC? Connecting via USB is easy and we show you

how to do that in the second video on the startup page of Do-more Designer. Connecting via Ethernet is just as easy, but

there are a couple different ways to do it and you have to make it compatible with your

existing Ethernet Network. Those steps are shown in this brief video. Number 2: When should you use a Task a Program

a subroutine or an ISR? Use a Program if you want to use Stages or

your logic takes multiple scans, like when doing communications or timers for example. Use a Task if you know your logic just needs

one pass through the code, even if it needs to be done over multiple scans. Create a subroutine for a function you want

to use over and over again and be able to pass variables to. And use Interrupt Service Routines for your

interrupt I/O. Number 3:

Ethernet I/O is an excellent way to get more I/O’s on your base PLC. You just plug a Do-more PLC with an Ethernet

port into a network with DirectLogic or Terminator bases with EBC controllers – not the regular

CPU’s- and enable the Ethernet I/O on the Do-more. You now have a ton of I/O that appear to the

Do-more as simple local I/O. If you want to learn more about Ethernet I/O check these

videos in the Do-more Video Library. Number 4: Modbus Communications. Connecting a Do-more PLC to a device via Modbus

is simple. It can be a Modbus Client or a Server and

it can use Modbus RTU over serial, or Modbus TCP over Ethernet. Number 5: PID

If you haven’t done it before, let’s face it - PID can be intimidating. The good news is Do-more PLCs make setting

up PID simple and straight forward. Do-more Designer even has tools to help you

visualize and tune the loops. This is a really big subject so look in the

video library for some tutorials on how to setup and use PID. Number 6: Casting

Have you ever had to take a word of data and pull a byte or one bit out of it for a comparison

or to format it for transfer? It’s a pain – right? Casting gives you a superfast shortcut around

all of those programming headaches. With casting you can convert any memory type

into any other on the fly without having to do a lot of math and bit shifting and byte

a swapping, and all that yucky stuff. The help topic covers every possible way you

can cast one thing into another so take a look at that to learn more. And check this out. In the element browser, this little button

down here is awesome. Suppose I want to take a V memory element

and pull one bit out of it. Look – it shows me the exact format I need

to use! How about a taking signed word and pulling

out a byte, the upper byte and we want it unsigned. There’s the exact format I need. So when in doubt, use the cast builder – it’s

quick and easy. Once you get the hang of it, casting will

quickly become one of your favorite programming tools. Number 7: Peerlink

Peerlink is one of the easiest ways to share data between any mix of Do-more PLCs and DirectLogic

PLCs. Number 8: Communications

Do-more PLCs have lots of ways to communicate with other PLCs and other devices. Again, The Do-more video library has step

by step examples showing how to use those so we’re not going to spend time on it here. If you didn’t see your favorite topic here,

then head over to the Do-more video library. Chances are, you’ll find what you are looking

for there. And if not, then please contact AutomationDirect’s

free award winning support team during regular business hours. They will be happy to help. And don’t forget the forums. There are lots of automation professionals

there that love to share their years of experience. Just don’t post any questions directed at

AutomationDirect’s support team there, they don’t monitor the forums on a regular basis. Spend Less, Do More, With AutomationDirect.


Playlist Not Found Could not find playlist PLPdypWXY_ROqT5KTqjfyhR7t0fD16Nya8

Playlist Not Found Could not find playlist PLPdypWXY_ROqvbaYVBWc3kH-pP01fI4-E

Playlist Not Found Could not find playlist PLPdypWXY_ROqJO86ikigKmjnSkbguBKBw

Playlist Not Found Could not find playlist PLPdypWXY_ROoqTZihvX8c8UUj5GzVCuKH

Playlist Not Found Could not find playlist PLPdypWXY_ROr0ZfCV-fAgau5yDemA19CV

Playlist Not Found Could not find playlist PLPdypWXY_ROqWWy8OnWGt3YD4Dald6uf-

BRX Do-more PLCs - Hardware
  • Video
    How To Sense Temperature with a Do-more PLC from AutomationDirect
  • Video
    How To Detect Objects with an AutomationDirect Do-more PLC
  • Video
    AC Motor On/Off with Do-more PLC Part 1 from AutomationDirect
  • Video
    AC Motor On/Off with Do-more PLC Part 2 from AutomationDirect
  • Video
    How to Sense Distance with an AutomationDirect Do-more PLC

Playlist Not Found Could not find playlist PLPdypWXY_ROrRJ5YuFYxs3mSXr9250AN7

Playlist Not Found Could not find playlist PLPdypWXY_ROrtSkGYNq8Xc52QWTCWf2Ci
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
Copyright © 1999-2025 AutomationDirect.  ALL RIGHTS RESERVED.
Site Map     Send Us your Feedback     Unsubscribe     Email Preferences     Legal & Business Policies     YouTube Terms of Service
Clear login credentials



Back to Top


spinner Updating...
Info