Filter Results Clear All
You've selected:
> Programmable Controllers > BRX PLCs (Stackable Micro Brick)
  •   Shop  
  •   Overview  
  •   In Depth  
BRX Home BRX - Your Automation Foundation Configure a BRX
 
Features
10 ways it's better with BRX PLCs! IIoT Edge Device: Your low cost link to Industry 4.0..and beyond! Not Your Everyday Analog Security Simple Data Logging/Advanced Data Control Fortified with American Pride Easy Migration Motion Control/Positioning made easy!
Free Software
What's New with Do-more Designer Dashboard- Easy Navigation Simulator Easy PID Auto-Discover I/O Powerful Math Troublefree Troubleshooting DirectLOGIC Migration Instruction Set Free Online Training Video Help Download the Free Software
Hardware
Hardware Overview M Series CPUs (no I/O) 10-point Series CPUs 18-point Series CPUs 36-point Series CPUs Ethernet Remote I/O Expansion Modules Pluggable Option Modules Connection Options Spare Parts Go to ZIPLink Selector Tool
Videos


BRX Series PLCs (Stackable Micro Brick) Videos

View Do-more Designer Video


Detailed Product
Overview



To learn more: https://www.automationdirect.com/do-more?utm_source=qhNTjcxXlpc&utm_medium=VideoTeamDescription - (VID-DM-0044)

Learn how to use Yielding to spread out the execution of programs and tasks that normally take a long time to execute so they have minimal impact on your scan time!
**Software Version used in this video: Do-more Designer 2.0.0

Online Support Page: https://community.automationdirect.com/s/contactsupport?utm_source=qhNTjcxXlpc&utm_medium=VideoTeamDescription

**Please check our website for our most up-to-date product pricing and availability.


Hide Transcript
View Transcript
Suppose you have a program or a task that

needs to take a lot of time, but you don’t want it to extend the main scan loop any more

than necessary. Maybe you are using a task to generate an

end of shift report and you have to loop through tons of records to build a log, or maybe you

need to respond to a communications event with a program and it’s going to take a

while to collect the data for the response. Those can take a long time and you really

don’t want them to slow down your scan loop to do it, right? Well, that’s where yielding comes in handy. The Do-more PLC lets you tell programs and

tasks to just do a little bit of the job each scan so your main process isn’t affected. Now, each scan is spending most of the time

taking care of your time critical main program. So Yielding is a great way to spread low priority

tasks and programs out over time to help keep your main program running as fast as possible. To use Yielding you just right click on the

program or task. If you choose never yield, a task and a program

will run to completion regardless of how long it takes. The only thing that can change that is if

you manually put a YIELD instruction in the code. Then the task or program will run to that

instruction on one scan, and then pick up there on the next scan. You can do that as many times as you want

to break up the task or program however you need. Always yield is basically the same thing,

except it will also yield for a GOTO instruction – if the GOTO instruction points to something

earlier in the code of course. Then on the next scan it will start at that

previous line and continue to the bottom of the routine. Assuming it doesn’t hit another GOTO again,

of course. And it will yield at the bottom of a loop:

for next loop, a while end loop or a do until loop. Which means under this Always YIELD option,

a program will run one iteration through the loop, then on the next scan run another iteration,

next scan another iteration, etc. That’s an easy way to tell programs and

tasks to run one iteration of a loop per scan. What if you have a loop inside a loop? Well, it will yield at the bottom of this

loop, and keep doing that until it’s done, then on the next scan it will pick up here

and yield at the bottom of this loop. Then on the next scan it will fall back into

this loop and repeat the whole process again. Exactly what you would expect. And finally, this option takes that one step

farther. Suppose you know you can afford for a Program

or a TASK to take, let’s say, 1 millisecond of scan time without adversely affecting your

main scan loop. Well, you put 1 millisecond here and now the

program or task will run as many loop iterations as it can until 1 millisecond expires, then

it will yield at the next yielding instruction which is usually the bottom of a loop. On the next scan it just picks up wherever

it left off. Runs as many loop iterations as it can in

the 1000 micro-seconds then yields again. Here’s something to think about: Can the

main program Yield? That is, could you break up the main program

so different parts run on different scans? Sure! The Main is just another program so all of

these option still apply. The only difference is the Main program always

runs – you can’t shut it down. Other than that, the Main Program acts just

like any user created program. But, if you are using Yielding to break up

your main program, that’s probably a pretty good sign that you need to be creating some

more programs and tasks. So Yielding gives you incredible control over

the performance of your system and its super easy to use! So be sure to take advantage of it when you

need to optimize your system’s performance. In the next video we’ll do some live examples

so you can get a better feel for the differences between tasks ad programs. If you have any questions, please contact

AutomationDirect’s free, award winning support team during regular business hours. They will be happy to help. And don’t forget the forums. There are lots of automation professionals

there that love to share their years of experience. Just don’t post any questions directed at

AutomationDirect’s support team there, they don’t monitor the forums on a regular basis. Spend Less, Do-more. With AutomationDirect.


Playlist Not Found Could not find playlist PLPdypWXY_ROqT5KTqjfyhR7t0fD16Nya8

Playlist Not Found Could not find playlist PLPdypWXY_ROqvbaYVBWc3kH-pP01fI4-E

Playlist Not Found Could not find playlist PLPdypWXY_ROqJO86ikigKmjnSkbguBKBw

Playlist Not Found Could not find playlist PLPdypWXY_ROoqTZihvX8c8UUj5GzVCuKH

Playlist Not Found Could not find playlist PLPdypWXY_ROr0ZfCV-fAgau5yDemA19CV

Playlist Not Found Could not find playlist PLPdypWXY_ROqWWy8OnWGt3YD4Dald6uf-

BRX Do-more PLCs - Hardware
  • Video
    How To Sense Temperature with a Do-more PLC from AutomationDirect
  • Video
    How To Detect Objects with an AutomationDirect Do-more PLC
  • Video
    AC Motor On/Off with Do-more PLC Part 1 from AutomationDirect
  • Video
    AC Motor On/Off with Do-more PLC Part 2 from AutomationDirect
  • Video
    How to Sense Distance with an AutomationDirect Do-more PLC

Playlist Not Found Could not find playlist PLPdypWXY_ROrRJ5YuFYxs3mSXr9250AN7

Playlist Not Found Could not find playlist PLPdypWXY_ROrtSkGYNq8Xc52QWTCWf2Ci